|
TI OAD API Documentation
9.14.02
|
Struct containing the parameters required for asset create and plaintext key load operations. More...
Data Fields | |
| HSMBareMetal_AESOperationMode | aesOperationMode |
| HSMBareMetal_operationAlgorithm | algorithm |
| HSMBareMetal_ECCOperationCurveType | eccCurveType |
| HSMBareMetal_ECCKeyType | eccKeyType |
| HSMBareMetal_ECCOperationMode | eccOperationMode |
| bool | isKeyGenerated |
| uint8_t * | key |
| HSMBareMetal_AssetPairStruct | keyAssetIDs |
| uint8_t * | keyblob |
| uint8_t | keyLength |
| HSMBareMetal_MACOperationMode | macOperationMode |
| HSMBareMetal_operationDirection | operationDirection |
| HSMBareMetal_AssetOperationType | operationType |
Struct containing the parameters required for asset create and plaintext key load operations.
1.8.12