TI OAD API Documentation  9.14.02
Macros | Typedefs | Functions
Key derivation and pseudorandom generation

Macros

#define PSA_KEY_DERIVATION_UNLIMITED_CAPACITY   ((size_t) (-1))
 

Typedefs

typedef struct psa_key_derivation_s psa_key_derivation_operation_t
 

Functions

psa_status_t psa_key_derivation_abort (psa_key_derivation_operation_t *operation)
 
psa_status_t psa_key_derivation_get_capacity (const psa_key_derivation_operation_t *operation, size_t *capacity)
 
psa_status_t psa_key_derivation_input_bytes (psa_key_derivation_operation_t *operation, psa_key_derivation_step_t step, const uint8_t *data, size_t data_length)
 
psa_status_t psa_key_derivation_input_integer (psa_key_derivation_operation_t *operation, psa_key_derivation_step_t step, uint64_t value)
 
psa_status_t psa_key_derivation_input_key (psa_key_derivation_operation_t *operation, psa_key_derivation_step_t step, psa_key_id_t key)
 
psa_status_t psa_key_derivation_key_agreement (psa_key_derivation_operation_t *operation, psa_key_derivation_step_t step, psa_key_id_t private_key, const uint8_t *peer_key, size_t peer_key_length)
 
psa_status_t psa_key_derivation_output_bytes (psa_key_derivation_operation_t *operation, uint8_t *output, size_t output_length)
 
psa_status_t psa_key_derivation_output_key (const psa_key_attributes_t *attributes, psa_key_derivation_operation_t *operation, psa_key_id_t *key)
 
psa_status_t psa_key_derivation_set_capacity (psa_key_derivation_operation_t *operation, size_t capacity)
 
psa_status_t psa_key_derivation_setup (psa_key_derivation_operation_t *operation, psa_algorithm_t alg)
 
psa_status_t psa_key_derivation_verify_bytes (psa_key_derivation_operation_t *operation, const uint8_t *expected_output, size_t output_length)
 
psa_status_t psa_key_derivation_verify_key (psa_key_derivation_operation_t *operation, psa_key_id_t expected)
 
psa_status_t psa_raw_key_agreement (psa_algorithm_t alg, psa_key_id_t private_key, const uint8_t *peer_key, size_t peer_key_length, uint8_t *output, size_t output_size, size_t *output_length)
 

Detailed Description

Macro Definition Documentation

§ PSA_KEY_DERIVATION_UNLIMITED_CAPACITY

#define PSA_KEY_DERIVATION_UNLIMITED_CAPACITY   ((size_t) (-1))

Use the maximum possible capacity for a key derivation operation.

Use this value as the capacity argument when setting up a key derivation to indicate that the operation should have the maximum possible capacity. The value of the maximum possible capacity depends on the key derivation algorithm.

Typedef Documentation

§ psa_key_derivation_operation_t

typedef struct psa_key_derivation_s psa_key_derivation_operation_t

The type of the state data structure for key derivation operations.

Before calling any function on a key derivation operation object, the application must initialize it by any of the following means:

  • Set the structure to all-bits-zero, for example:
    memset(&operation, 0, sizeof(operation));
  • Initialize the structure to logical zero values, for example:
  • Initialize the structure to the initializer #PSA_KEY_DERIVATION_OPERATION_INIT, for example:
    psa_key_derivation_operation_t operation = PSA_KEY_DERIVATION_OPERATION_INIT;
  • Assign the result of the function psa_key_derivation_operation_init() to the structure, for example:
    operation = psa_key_derivation_operation_init();

This is an implementation-defined struct. Applications should not make any assumptions about the content of this structure. Implementation details can change in future versions without notice.

Function Documentation

§ psa_key_derivation_abort()

psa_status_t psa_key_derivation_abort ( psa_key_derivation_operation_t operation)

Abort a key derivation operation.

Aborting an operation frees all associated resources except for the operation structure itself. Once aborted, the operation object can be reused for another operation by calling psa_key_derivation_setup() again.

This function may be called at any time after the operation object has been initialized as described in psa_key_derivation_operation_t.

In particular, it is valid to call psa_key_derivation_abort() twice, or to call psa_key_derivation_abort() on an operation that has not been set up.

Parameters
[in,out]operationThe operation to abort.
Return values
#PSA_SUCCESS
#PSA_ERROR_COMMUNICATION_FAILURE
#PSA_ERROR_HARDWARE_FAILURE
#PSA_ERROR_CORRUPTION_DETECTED
#PSA_ERROR_BAD_STATEThe library has not been previously initialized by psa_crypto_init(). It is implementation-dependent whether a failure to initialize results in this error code.

§ psa_key_derivation_get_capacity()

psa_status_t psa_key_derivation_get_capacity ( const psa_key_derivation_operation_t operation,
size_t *  capacity 
)

Retrieve the current capacity of a key derivation operation.

The capacity of a key derivation is the maximum number of bytes that it can return. When you get N bytes of output from a key derivation operation, this reduces its capacity by N.

Parameters
[in]operationThe operation to query.
[out]capacityOn success, the capacity of the operation.
Return values
#PSA_SUCCESS
#PSA_ERROR_COMMUNICATION_FAILURE
#PSA_ERROR_HARDWARE_FAILURE
#PSA_ERROR_CORRUPTION_DETECTED
#PSA_ERROR_BAD_STATEThe operation state is not valid (it must be active), or the library has not been previously initialized by psa_crypto_init(). It is implementation-dependent whether a failure to initialize results in this error code.

§ psa_key_derivation_input_bytes()

psa_status_t psa_key_derivation_input_bytes ( psa_key_derivation_operation_t operation,
psa_key_derivation_step_t  step,
const uint8_t *  data,
size_t  data_length 
)

Provide an input for key derivation or key agreement.

Which inputs are required and in what order depends on the algorithm. Refer to the documentation of each key derivation or key agreement algorithm for information.

This function passes direct inputs, which is usually correct for non-secret inputs. To pass a secret input, which should be in a key object, call psa_key_derivation_input_key() instead of this function. Refer to the documentation of individual step types (PSA_KEY_DERIVATION_INPUT_xxx values of type ::psa_key_derivation_step_t) for more information.

If this function returns an error status, the operation enters an error state and must be aborted by calling psa_key_derivation_abort().

Parameters
[in,out]operationThe key derivation operation object to use. It must have been set up with psa_key_derivation_setup() and must not have produced any output yet.
stepWhich step the input data is for.
[in]dataInput data to use.
data_lengthSize of the data buffer in bytes.
Return values
#PSA_SUCCESSSuccess.
#PSA_ERROR_INVALID_ARGUMENTstep is not compatible with the operation's algorithm, or step does not allow direct inputs.
#PSA_ERROR_INSUFFICIENT_MEMORY
#PSA_ERROR_COMMUNICATION_FAILURE
#PSA_ERROR_HARDWARE_FAILURE
#PSA_ERROR_CORRUPTION_DETECTED
#PSA_ERROR_STORAGE_FAILURE
#PSA_ERROR_BAD_STATEThe operation state is not valid for this input step, or the library has not been previously initialized by psa_crypto_init(). It is implementation-dependent whether a failure to initialize results in this error code.

§ psa_key_derivation_input_integer()

psa_status_t psa_key_derivation_input_integer ( psa_key_derivation_operation_t operation,
psa_key_derivation_step_t  step,
uint64_t  value 
)

Provide a numeric input for key derivation or key agreement.

Which inputs are required and in what order depends on the algorithm. However, when an algorithm requires a particular order, numeric inputs usually come first as they tend to be configuration parameters. Refer to the documentation of each key derivation or key agreement algorithm for information.

This function is used for inputs which are fixed-size non-negative integers.

If this function returns an error status, the operation enters an error state and must be aborted by calling psa_key_derivation_abort().

Parameters
[in,out]operationThe key derivation operation object to use. It must have been set up with psa_key_derivation_setup() and must not have produced any output yet.
stepWhich step the input data is for.
[in]valueThe value of the numeric input.
Return values
#PSA_SUCCESSSuccess.
#PSA_ERROR_INVALID_ARGUMENTstep is not compatible with the operation's algorithm, or step does not allow numeric inputs.
#PSA_ERROR_INSUFFICIENT_MEMORY
#PSA_ERROR_COMMUNICATION_FAILURE
#PSA_ERROR_HARDWARE_FAILURE
#PSA_ERROR_CORRUPTION_DETECTED
#PSA_ERROR_STORAGE_FAILURE
#PSA_ERROR_BAD_STATEThe operation state is not valid for this input step, or the library has not been previously initialized by psa_crypto_init(). It is implementation-dependent whether a failure to initialize results in this error code.

§ psa_key_derivation_input_key()

psa_status_t psa_key_derivation_input_key ( psa_key_derivation_operation_t operation,
psa_key_derivation_step_t  step,
psa_key_id_t  key 
)

Provide an input for key derivation in the form of a key.

Which inputs are required and in what order depends on the algorithm. Refer to the documentation of each key derivation or key agreement algorithm for information.

This function obtains input from a key object, which is usually correct for secret inputs or for non-secret personalization strings kept in the key store. To pass a non-secret parameter which is not in the key store, call psa_key_derivation_input_bytes() instead of this function. Refer to the documentation of individual step types (PSA_KEY_DERIVATION_INPUT_xxx values of type ::psa_key_derivation_step_t) for more information.

If this function returns an error status, the operation enters an error state and must be aborted by calling psa_key_derivation_abort().

Parameters
[in,out]operationThe key derivation operation object to use. It must have been set up with psa_key_derivation_setup() and must not have produced any output yet.
stepWhich step the input data is for.
keyIdentifier of the key. It must have an appropriate type for step and must allow the usage #PSA_KEY_USAGE_DERIVE or #PSA_KEY_USAGE_VERIFY_DERIVATION (see note) and the algorithm used by the operation.
Note
Once all inputs steps are completed, the operations will allow:
Return values
#PSA_SUCCESSSuccess.
#PSA_ERROR_INVALID_HANDLE
#PSA_ERROR_NOT_PERMITTEDThe key allows neither #PSA_KEY_USAGE_DERIVE nor #PSA_KEY_USAGE_VERIFY_DERIVATION, or it doesn't allow this algorithm.
#PSA_ERROR_INVALID_ARGUMENTstep is not compatible with the operation's algorithm, or step does not allow key inputs of the given type or does not allow key inputs at all.
#PSA_ERROR_INSUFFICIENT_MEMORY
#PSA_ERROR_COMMUNICATION_FAILURE
#PSA_ERROR_HARDWARE_FAILURE
#PSA_ERROR_CORRUPTION_DETECTED
#PSA_ERROR_STORAGE_FAILURE
#PSA_ERROR_BAD_STATEThe operation state is not valid for this input step, or the library has not been previously initialized by psa_crypto_init(). It is implementation-dependent whether a failure to initialize results in this error code.

§ psa_key_derivation_key_agreement()

psa_status_t psa_key_derivation_key_agreement ( psa_key_derivation_operation_t operation,
psa_key_derivation_step_t  step,
psa_key_id_t  private_key,
const uint8_t *  peer_key,
size_t  peer_key_length 
)

Perform a key agreement and use the shared secret as input to a key derivation.

A key agreement algorithm takes two inputs: a private key private_key a public key peer_key. The result of this function is passed as input to a key derivation. The output of this key derivation can be extracted by reading from the resulting operation to produce keys and other cryptographic material.

If this function returns an error status, the operation enters an error state and must be aborted by calling psa_key_derivation_abort().

Parameters
[in,out]operationThe key derivation operation object to use. It must have been set up with psa_key_derivation_setup() with a key agreement and derivation algorithm alg (PSA_ALG_XXX value such that #PSA_ALG_IS_KEY_AGREEMENT(alg) is true and #PSA_ALG_IS_RAW_KEY_AGREEMENT(alg) is false). The operation must be ready for an input of the type given by step.
stepWhich step the input data is for.
private_keyIdentifier of the private key to use. It must allow the usage #PSA_KEY_USAGE_DERIVE.
[in]peer_keyPublic key of the peer. The peer key must be in the same format that psa_import_key() accepts for the public key type corresponding to the type of private_key. That is, this function performs the equivalent of psa_import_key(..., peer_key, peer_key_length) where with key attributes indicating the public key type corresponding to the type of private_key. For example, for EC keys, this means that peer_key is interpreted as a point on the curve that the private key is on. The standard formats for public keys are documented in the documentation of psa_export_public_key().
peer_key_lengthSize of peer_key in bytes.
Return values
#PSA_SUCCESSSuccess.
#PSA_ERROR_INVALID_HANDLE
#PSA_ERROR_NOT_PERMITTED
#PSA_ERROR_INVALID_ARGUMENTprivate_key is not compatible with alg, or peer_key is not valid for alg or not compatible with private_key, or step does not allow an input resulting from a key agreement.
#PSA_ERROR_NOT_SUPPORTEDalg is not supported or is not a key derivation algorithm.
#PSA_ERROR_INSUFFICIENT_MEMORY
#PSA_ERROR_COMMUNICATION_FAILURE
#PSA_ERROR_HARDWARE_FAILURE
#PSA_ERROR_CORRUPTION_DETECTED
#PSA_ERROR_STORAGE_FAILURE
#PSA_ERROR_BAD_STATEThe operation state is not valid for this key agreement step, or the library has not been previously initialized by psa_crypto_init(). It is implementation-dependent whether a failure to initialize results in this error code.

§ psa_key_derivation_output_bytes()

psa_status_t psa_key_derivation_output_bytes ( psa_key_derivation_operation_t operation,
uint8_t *  output,
size_t  output_length 
)

Read some data from a key derivation operation.

This function calculates output bytes from a key derivation algorithm and return those bytes. If you view the key derivation's output as a stream of bytes, this function destructively reads the requested number of bytes from the stream. The operation's capacity decreases by the number of bytes read.

If this function returns an error status other than #PSA_ERROR_INSUFFICIENT_DATA, the operation enters an error state and must be aborted by calling psa_key_derivation_abort().

Parameters
[in,out]operationThe key derivation operation object to read from.
[out]outputBuffer where the output will be written.
output_lengthNumber of bytes to output.
Return values
#PSA_SUCCESS
#PSA_ERROR_NOT_PERMITTEDOne of the inputs was a key whose policy didn't allow #PSA_KEY_USAGE_DERIVE.
#PSA_ERROR_INSUFFICIENT_DATAThe operation's capacity was less than output_length bytes. Note that in this case, no output is written to the output buffer. The operation's capacity is set to 0, thus subsequent calls to this function will not succeed, even with a smaller output buffer.
#PSA_ERROR_INSUFFICIENT_MEMORY
#PSA_ERROR_COMMUNICATION_FAILURE
#PSA_ERROR_HARDWARE_FAILURE
#PSA_ERROR_CORRUPTION_DETECTED
#PSA_ERROR_STORAGE_FAILURE
#PSA_ERROR_BAD_STATEThe operation state is not valid (it must be active and completed all required input steps), or the library has not been previously initialized by psa_crypto_init(). It is implementation-dependent whether a failure to initialize results in this error code.

§ psa_key_derivation_output_key()

psa_status_t psa_key_derivation_output_key ( const psa_key_attributes_t *  attributes,
psa_key_derivation_operation_t operation,
psa_key_id_t *  key 
)

Derive a key from an ongoing key derivation operation.

This function calculates output bytes from a key derivation algorithm and uses those bytes to generate a key deterministically. The key's location, usage policy, type and size are taken from attributes.

If you view the key derivation's output as a stream of bytes, this function destructively reads as many bytes as required from the stream. The operation's capacity decreases by the number of bytes read.

If this function returns an error status other than #PSA_ERROR_INSUFFICIENT_DATA, the operation enters an error state and must be aborted by calling psa_key_derivation_abort().

How much output is produced and consumed from the operation, and how the key is derived, depends on the key type and on the key size (denoted bits below):

  • For key types for which the key is an arbitrary sequence of bytes of a given size, this function is functionally equivalent to calling psa_key_derivation_output_bytes and passing the resulting output to psa_import_key. However, this function has a security benefit: if the implementation provides an isolation boundary then the key material is not exposed outside the isolation boundary. As a consequence, for these key types, this function always consumes exactly (bits / 8) bytes from the operation. The following key types defined in this specification follow this scheme:
    • #PSA_KEY_TYPE_AES;
    • #PSA_KEY_TYPE_ARIA;
    • #PSA_KEY_TYPE_CAMELLIA;
    • #PSA_KEY_TYPE_DERIVE;
    • #PSA_KEY_TYPE_HMAC;
    • #PSA_KEY_TYPE_PASSWORD_HASH.
  • For ECC keys on a Montgomery elliptic curve (#PSA_KEY_TYPE_ECC_KEY_PAIR(curve) where curve designates a Montgomery curve), this function always draws a byte string whose length is determined by the curve, and sets the mandatory bits accordingly. That is:
    • Curve25519 (#PSA_ECC_FAMILY_MONTGOMERY, 255 bits): draw a 32-byte string and process it as specified in RFC 7748 §5.
    • Curve448 (#PSA_ECC_FAMILY_MONTGOMERY, 448 bits): draw a 56-byte string and process it as specified in RFC 7748 §5.
  • For key types for which the key is represented by a single sequence of bits bits with constraints as to which bit sequences are acceptable, this function draws a byte string of length (bits / 8) bytes rounded up to the nearest whole number of bytes. If the resulting byte string is acceptable, it becomes the key, otherwise the drawn bytes are discarded. This process is repeated until an acceptable byte string is drawn. The byte string drawn from the operation is interpreted as specified for the output produced by psa_export_key(). The following key types defined in this specification follow this scheme:
    • #PSA_KEY_TYPE_DES. Force-set the parity bits, but discard forbidden weak keys. For 2-key and 3-key triple-DES, the three keys are generated successively (for example, for 3-key triple-DES, if the first 8 bytes specify a weak key and the next 8 bytes do not, discard the first 8 bytes, use the next 8 bytes as the first key, and continue reading output from the operation to derive the other two keys).
    • Finite-field Diffie-Hellman keys (#PSA_KEY_TYPE_DH_KEY_PAIR(group) where group designates any Diffie-Hellman group) and ECC keys on a Weierstrass elliptic curve (#PSA_KEY_TYPE_ECC_KEY_PAIR(curve) where curve designates a Weierstrass curve). For these key types, interpret the byte string as integer in big-endian order. Discard it if it is not in the range [0, N - 2] where N is the boundary of the private key domain (the prime p for Diffie-Hellman, the subprime q for DSA, or the order of the curve's base point for ECC). Add 1 to the resulting integer and use this as the private key x. This method allows compliance to NIST standards, specifically the methods titled "key-pair generation by testing candidates" in NIST SP 800-56A §5.6.1.1.4 for Diffie-Hellman, in FIPS 186-4 §B.1.2 for DSA, and in NIST SP 800-56A §5.6.1.2.2 or FIPS 186-4 §B.4.2 for elliptic curve keys.
  • For other key types, including #PSA_KEY_TYPE_RSA_KEY_PAIR, the way in which the operation output is consumed is implementation-defined.

In all cases, the data that is read is discarded from the operation. The operation's capacity is decreased by the number of bytes read.

For algorithms that take an input step #PSA_KEY_DERIVATION_INPUT_SECRET, the input to that step must be provided with psa_key_derivation_input_key(). Future versions of this specification may include additional restrictions on the derived key based on the attributes and strength of the secret key.

Parameters
[in]attributesThe attributes for the new key. If the key type to be created is #PSA_KEY_TYPE_PASSWORD_HASH then the algorithm in the policy must be the same as in the current operation.
[in,out]operationThe key derivation operation object to read from.
[out]keyOn success, an identifier for the newly created key. For persistent keys, this is the key identifier defined in attributes. 0 on failure.
Return values
#PSA_SUCCESSSuccess. If the key is persistent, the key material and the key's metadata have been saved to persistent storage.
#PSA_ERROR_ALREADY_EXISTSThis is an attempt to create a persistent key, and there is already a persistent key with the given identifier.
#PSA_ERROR_INSUFFICIENT_DATAThere was not enough data to create the desired key. Note that in this case, no output is written to the output buffer. The operation's capacity is set to 0, thus subsequent calls to this function will not succeed, even with a smaller output buffer.
#PSA_ERROR_NOT_SUPPORTEDThe key type or key size is not supported, either by the implementation in general or in this particular location.
#PSA_ERROR_INVALID_ARGUMENTThe provided key attributes are not valid for the operation.
#PSA_ERROR_NOT_PERMITTEDThe #PSA_KEY_DERIVATION_INPUT_SECRET or #PSA_KEY_DERIVATION_INPUT_PASSWORD input was not provided through a key; or one of the inputs was a key whose policy didn't allow #PSA_KEY_USAGE_DERIVE.
#PSA_ERROR_INSUFFICIENT_MEMORY
#PSA_ERROR_INSUFFICIENT_STORAGE
#PSA_ERROR_COMMUNICATION_FAILURE
#PSA_ERROR_HARDWARE_FAILURE
#PSA_ERROR_CORRUPTION_DETECTED
#PSA_ERROR_DATA_INVALID
#PSA_ERROR_DATA_CORRUPT
#PSA_ERROR_STORAGE_FAILURE
#PSA_ERROR_BAD_STATEThe operation state is not valid (it must be active and completed all required input steps), or the library has not been previously initialized by psa_crypto_init(). It is implementation-dependent whether a failure to initialize results in this error code.

§ psa_key_derivation_set_capacity()

psa_status_t psa_key_derivation_set_capacity ( psa_key_derivation_operation_t operation,
size_t  capacity 
)

Set the maximum capacity of a key derivation operation.

The capacity of a key derivation operation is the maximum number of bytes that the key derivation operation can return from this point onwards.

Parameters
[in,out]operationThe key derivation operation object to modify.
capacityThe new capacity of the operation. It must be less or equal to the operation's current capacity.
Return values
#PSA_SUCCESS
#PSA_ERROR_INVALID_ARGUMENTcapacity is larger than the operation's current capacity. In this case, the operation object remains valid and its capacity remains unchanged.
#PSA_ERROR_COMMUNICATION_FAILURE
#PSA_ERROR_HARDWARE_FAILURE
#PSA_ERROR_CORRUPTION_DETECTED
#PSA_ERROR_BAD_STATEThe operation state is not valid (it must be active), or the library has not been previously initialized by psa_crypto_init(). It is implementation-dependent whether a failure to initialize results in this error code.

§ psa_key_derivation_setup()

psa_status_t psa_key_derivation_setup ( psa_key_derivation_operation_t operation,
psa_algorithm_t  alg 
)

Set up a key derivation operation.

A key derivation algorithm takes some inputs and uses them to generate a byte stream in a deterministic way. This byte stream can be used to produce keys and other cryptographic material.

To derive a key:

  1. Start with an initialized object of type psa_key_derivation_operation_t.
  2. Call psa_key_derivation_setup() to select the algorithm.
  3. Provide the inputs for the key derivation by calling psa_key_derivation_input_bytes() or psa_key_derivation_input_key() as appropriate. Which inputs are needed, in what order, and whether they may be keys and if so of what type depends on the algorithm.
  4. Optionally set the operation's maximum capacity with psa_key_derivation_set_capacity(). You may do this before, in the middle of or after providing inputs. For some algorithms, this step is mandatory because the output depends on the maximum capacity.
  5. To derive a key, call psa_key_derivation_output_key(). To derive a byte string for a different purpose, call psa_key_derivation_output_bytes(). Successive calls to these functions use successive output bytes calculated by the key derivation algorithm.
  6. Clean up the key derivation operation object with psa_key_derivation_abort().

If this function returns an error, the key derivation operation object is not changed.

If an error occurs at any step after a call to psa_key_derivation_setup(), the operation will need to be reset by a call to psa_key_derivation_abort().

Implementations must reject an attempt to derive a key of size 0.

Parameters
[in,out]operationThe key derivation operation object to set up. It must have been initialized but not set up yet.
algThe key derivation algorithm to compute (PSA_ALG_XXX value such that #PSA_ALG_IS_KEY_DERIVATION(alg) is true).
Return values
#PSA_SUCCESSSuccess.
#PSA_ERROR_INVALID_ARGUMENTalg is not a key derivation algorithm.
#PSA_ERROR_NOT_SUPPORTEDalg is not supported or is not a key derivation algorithm.
#PSA_ERROR_INSUFFICIENT_MEMORY
#PSA_ERROR_COMMUNICATION_FAILURE
#PSA_ERROR_HARDWARE_FAILURE
#PSA_ERROR_CORRUPTION_DETECTED
#PSA_ERROR_STORAGE_FAILURE
#PSA_ERROR_BAD_STATEThe operation state is not valid (it must be inactive), or the library has not been previously initialized by psa_crypto_init(). It is implementation-dependent whether a failure to initialize results in this error code.

§ psa_key_derivation_verify_bytes()

psa_status_t psa_key_derivation_verify_bytes ( psa_key_derivation_operation_t operation,
const uint8_t *  expected_output,
size_t  output_length 
)

Compare output data from a key derivation operation to an expected value.

This function calculates output bytes from a key derivation algorithm and compares those bytes to an expected value in constant time. If you view the key derivation's output as a stream of bytes, this function destructively reads the expected number of bytes from the stream before comparing them. The operation's capacity decreases by the number of bytes read.

This is functionally equivalent to the following code:

psa_key_derivation_output_bytes(operation, tmp, output_length);
if (memcmp(output, tmp, output_length) != 0)
return PSA_ERROR_INVALID_SIGNATURE;

except (1) it works even if the key's policy does not allow outputting the bytes, and (2) the comparison will be done in constant time.

If this function returns an error status other than #PSA_ERROR_INSUFFICIENT_DATA or #PSA_ERROR_INVALID_SIGNATURE, the operation enters an error state and must be aborted by calling psa_key_derivation_abort().

Parameters
[in,out]operationThe key derivation operation object to read from.
[in]expected_outputBuffer containing the expected derivation output.
output_lengthLength of the expected output; this is also the number of bytes that will be read.
Return values
#PSA_SUCCESS
#PSA_ERROR_INVALID_SIGNATUREThe output was read successfully, but it differs from the expected output.
#PSA_ERROR_NOT_PERMITTEDOne of the inputs was a key whose policy didn't allow #PSA_KEY_USAGE_VERIFY_DERIVATION.
#PSA_ERROR_INSUFFICIENT_DATAThe operation's capacity was less than output_length bytes. Note that in this case, the operation's capacity is set to 0, thus subsequent calls to this function will not succeed, even with a smaller expected output.
#PSA_ERROR_INSUFFICIENT_MEMORY
#PSA_ERROR_COMMUNICATION_FAILURE
#PSA_ERROR_HARDWARE_FAILURE
#PSA_ERROR_CORRUPTION_DETECTED
#PSA_ERROR_STORAGE_FAILURE
#PSA_ERROR_BAD_STATEThe operation state is not valid (it must be active and completed all required input steps), or the library has not been previously initialized by psa_crypto_init(). It is implementation-dependent whether a failure to initialize results in this error code.

§ psa_key_derivation_verify_key()

psa_status_t psa_key_derivation_verify_key ( psa_key_derivation_operation_t operation,
psa_key_id_t  expected 
)

Compare output data from a key derivation operation to an expected value stored in a key object.

This function calculates output bytes from a key derivation algorithm and compares those bytes to an expected value, provided as key of type #PSA_KEY_TYPE_PASSWORD_HASH. If you view the key derivation's output as a stream of bytes, this function destructively reads the number of bytes corresponding to the length of the expected value from the stream before comparing them. The operation's capacity decreases by the number of bytes read.

This is functionally equivalent to exporting the key and calling psa_key_derivation_verify_bytes() on the result, except that it works even if the key cannot be exported.

If this function returns an error status other than #PSA_ERROR_INSUFFICIENT_DATA or #PSA_ERROR_INVALID_SIGNATURE, the operation enters an error state and must be aborted by calling psa_key_derivation_abort().

Parameters
[in,out]operationThe key derivation operation object to read from.
[in]expectedA key of type #PSA_KEY_TYPE_PASSWORD_HASH containing the expected output. Its policy must include the #PSA_KEY_USAGE_VERIFY_DERIVATION flag and the permitted algorithm must match the operation. The value of this key was likely computed by a previous call to psa_key_derivation_output_key().
Return values
#PSA_SUCCESS
#PSA_ERROR_INVALID_SIGNATUREThe output was read successfully, but if differs from the expected output.
#PSA_ERROR_INVALID_HANDLEThe key passed as the expected value does not exist.
#PSA_ERROR_INVALID_ARGUMENTThe key passed as the expected value has an invalid type.
#PSA_ERROR_NOT_PERMITTEDThe key passed as the expected value does not allow this usage or this algorithm; or one of the inputs was a key whose policy didn't allow #PSA_KEY_USAGE_VERIFY_DERIVATION.
#PSA_ERROR_INSUFFICIENT_DATAThe operation's capacity was less than the length of the expected value. In this case, the operation's capacity is set to 0, thus subsequent calls to this function will not succeed, even with a smaller expected output.
#PSA_ERROR_INSUFFICIENT_MEMORY
#PSA_ERROR_COMMUNICATION_FAILURE
#PSA_ERROR_HARDWARE_FAILURE
#PSA_ERROR_CORRUPTION_DETECTED
#PSA_ERROR_STORAGE_FAILURE
#PSA_ERROR_BAD_STATEThe operation state is not valid (it must be active and completed all required input steps), or the library has not been previously initialized by psa_crypto_init(). It is implementation-dependent whether a failure to initialize results in this error code.

§ psa_raw_key_agreement()

psa_status_t psa_raw_key_agreement ( psa_algorithm_t  alg,
psa_key_id_t  private_key,
const uint8_t *  peer_key,
size_t  peer_key_length,
uint8_t *  output,
size_t  output_size,
size_t *  output_length 
)

Perform a key agreement and return the raw shared secret.

Warning
The raw result of a key agreement algorithm such as finite-field Diffie-Hellman or elliptic curve Diffie-Hellman has biases and should not be used directly as key material. It should instead be passed as input to a key derivation algorithm. To chain a key agreement with a key derivation, use psa_key_derivation_key_agreement() and other functions from the key derivation interface.
Parameters
algThe key agreement algorithm to compute (PSA_ALG_XXX value such that #PSA_ALG_IS_RAW_KEY_AGREEMENT(alg) is true).
private_keyIdentifier of the private key to use. It must allow the usage #PSA_KEY_USAGE_DERIVE.
[in]peer_keyPublic key of the peer. It must be in the same format that psa_import_key() accepts. The standard formats for public keys are documented in the documentation of psa_export_public_key().
peer_key_lengthSize of peer_key in bytes.
[out]outputBuffer where the decrypted message is to be written.
output_sizeSize of the output buffer in bytes.
[out]output_lengthOn success, the number of bytes that make up the returned output.
Return values
#PSA_SUCCESSSuccess.
#PSA_ERROR_INVALID_HANDLE
#PSA_ERROR_NOT_PERMITTED
#PSA_ERROR_INVALID_ARGUMENTalg is not a key agreement algorithm, or private_key is not compatible with alg, or peer_key is not valid for alg or not compatible with private_key.
#PSA_ERROR_BUFFER_TOO_SMALLoutput_size is too small
#PSA_ERROR_NOT_SUPPORTEDalg is not a supported key agreement algorithm.
#PSA_ERROR_INSUFFICIENT_MEMORY
#PSA_ERROR_COMMUNICATION_FAILURE
#PSA_ERROR_HARDWARE_FAILURE
#PSA_ERROR_CORRUPTION_DETECTED
#PSA_ERROR_STORAGE_FAILURE
#PSA_ERROR_BAD_STATEThe library has not been previously initialized by psa_crypto_init(). It is implementation-dependent whether a failure to initialize results in this error code.