TI OAD API Documentation  9.14.02
Functions
Library initialization

Functions

psa_status_t psa_crypto_init (void)
 Library initialization. More...
 

Detailed Description

Function Documentation

§ psa_crypto_init()

psa_status_t psa_crypto_init ( void  )

Library initialization.

Applications must call this function before calling any other function in this module.

Applications may call this function more than once. Once a call succeeds, subsequent calls are guaranteed to succeed.

If the application calls other functions before calling psa_crypto_init(), the behavior is undefined. Implementations are encouraged to either perform the operation as if the library had been initialized or to return #PSA_ERROR_BAD_STATE or some other applicable error. In particular, implementations should not return a success status if the lack of initialization may have security implications, for example due to improper seeding of the random number generator.

Return values
#PSA_SUCCESS
#PSA_ERROR_INSUFFICIENT_MEMORY
#PSA_ERROR_INSUFFICIENT_STORAGE
#PSA_ERROR_COMMUNICATION_FAILURE
#PSA_ERROR_HARDWARE_FAILURE
#PSA_ERROR_CORRUPTION_DETECTED
#PSA_ERROR_INSUFFICIENT_ENTROPY
#PSA_ERROR_STORAGE_FAILURE
#PSA_ERROR_DATA_INVALID
#PSA_ERROR_DATA_CORRUPT