|
TI OAD API Documentation
9.14.02
|
Functions | |
| psa_status_t | psa_asymmetric_decrypt (psa_key_id_t key, psa_algorithm_t alg, const uint8_t *input, size_t input_length, const uint8_t *salt, size_t salt_length, uint8_t *output, size_t output_size, size_t *output_length) |
| Decrypt a short message with a private key. More... | |
| psa_status_t | psa_asymmetric_encrypt (psa_key_id_t key, psa_algorithm_t alg, const uint8_t *input, size_t input_length, const uint8_t *salt, size_t salt_length, uint8_t *output, size_t output_size, size_t *output_length) |
| Encrypt a short message with a public key. More... | |
| psa_status_t | psa_sign_hash (psa_key_id_t key, psa_algorithm_t alg, const uint8_t *hash, size_t hash_length, uint8_t *signature, size_t signature_size, size_t *signature_length) |
| Sign a hash or short message with a private key. More... | |
| psa_status_t | psa_sign_message (psa_key_id_t key, psa_algorithm_t alg, const uint8_t *input, size_t input_length, uint8_t *signature, size_t signature_size, size_t *signature_length) |
| Sign a message with a private key. For hash-and-sign algorithms, this includes the hashing step. More... | |
| psa_status_t | psa_verify_hash (psa_key_id_t key, psa_algorithm_t alg, const uint8_t *hash, size_t hash_length, const uint8_t *signature, size_t signature_length) |
| Verify the signature of a hash or short message using a public key. More... | |
| psa_status_t | psa_verify_message (psa_key_id_t key, psa_algorithm_t alg, const uint8_t *input, size_t input_length, const uint8_t *signature, size_t signature_length) |
| Verify the signature of a message with a public key, using a hash-and-sign verification algorithm. More... | |
| psa_status_t psa_asymmetric_decrypt | ( | psa_key_id_t | key, |
| psa_algorithm_t | alg, | ||
| const uint8_t * | input, | ||
| size_t | input_length, | ||
| const uint8_t * | salt, | ||
| size_t | salt_length, | ||
| uint8_t * | output, | ||
| size_t | output_size, | ||
| size_t * | output_length | ||
| ) |
Decrypt a short message with a private key.
| key | Identifier of the key to use for the operation. It must be an asymmetric key pair. It must allow the usage #PSA_KEY_USAGE_DECRYPT. | |
| alg | An asymmetric encryption algorithm that is compatible with the type of key. | |
| [in] | input | The message to decrypt. |
| input_length | Size of the input buffer in bytes. | |
| [in] | salt | A salt or label, if supported by the encryption algorithm. If the algorithm does not support a salt, pass NULL. If the algorithm supports an optional salt and you do not want to pass a salt, pass NULL. |
| salt_length | Size of the salt buffer in bytes. If salt is NULL, pass 0. | |
| [out] | output | Buffer where the decrypted message is to be written. |
| output_size | Size of the output buffer in bytes. | |
| [out] | output_length | On success, the number of bytes that make up the returned output. |
| #PSA_SUCCESS | |
| #PSA_ERROR_INVALID_HANDLE | |
| #PSA_ERROR_NOT_PERMITTED | |
| #PSA_ERROR_BUFFER_TOO_SMALL | The size of the output buffer is too small. You can determine a sufficient buffer size by calling #PSA_ASYMMETRIC_DECRYPT_OUTPUT_SIZE(key_type, key_bits, alg) where key_type and key_bits are the type and bit-size respectively of key. |
| #PSA_ERROR_NOT_SUPPORTED | |
| #PSA_ERROR_INVALID_ARGUMENT | |
| #PSA_ERROR_INSUFFICIENT_MEMORY | |
| #PSA_ERROR_COMMUNICATION_FAILURE | |
| #PSA_ERROR_HARDWARE_FAILURE | |
| #PSA_ERROR_CORRUPTION_DETECTED | |
| #PSA_ERROR_STORAGE_FAILURE | |
| #PSA_ERROR_INSUFFICIENT_ENTROPY | |
| #PSA_ERROR_INVALID_PADDING | |
| #PSA_ERROR_BAD_STATE | The library has not been previously initialized by psa_crypto_init(). It is implementation-dependent whether a failure to initialize results in this error code. |
| psa_status_t psa_asymmetric_encrypt | ( | psa_key_id_t | key, |
| psa_algorithm_t | alg, | ||
| const uint8_t * | input, | ||
| size_t | input_length, | ||
| const uint8_t * | salt, | ||
| size_t | salt_length, | ||
| uint8_t * | output, | ||
| size_t | output_size, | ||
| size_t * | output_length | ||
| ) |
Encrypt a short message with a public key.
| key | Identifier of the key to use for the operation. It must be a public key or an asymmetric key pair. It must allow the usage #PSA_KEY_USAGE_ENCRYPT. | |
| alg | An asymmetric encryption algorithm that is compatible with the type of key. | |
| [in] | input | The message to encrypt. |
| input_length | Size of the input buffer in bytes. | |
| [in] | salt | A salt or label, if supported by the encryption algorithm. If the algorithm does not support a salt, pass NULL. If the algorithm supports an optional salt and you do not want to pass a salt, pass NULL. |
| salt_length | Size of the salt buffer in bytes. If salt is NULL, pass 0. | |
| [out] | output | Buffer where the encrypted message is to be written. |
| output_size | Size of the output buffer in bytes. | |
| [out] | output_length | On success, the number of bytes that make up the returned output. |
| #PSA_SUCCESS | |
| #PSA_ERROR_INVALID_HANDLE | |
| #PSA_ERROR_NOT_PERMITTED | |
| #PSA_ERROR_BUFFER_TOO_SMALL | The size of the output buffer is too small. You can determine a sufficient buffer size by calling #PSA_ASYMMETRIC_ENCRYPT_OUTPUT_SIZE(key_type, key_bits, alg) where key_type and key_bits are the type and bit-size respectively of key. |
| #PSA_ERROR_NOT_SUPPORTED | |
| #PSA_ERROR_INVALID_ARGUMENT | |
| #PSA_ERROR_INSUFFICIENT_MEMORY | |
| #PSA_ERROR_COMMUNICATION_FAILURE | |
| #PSA_ERROR_HARDWARE_FAILURE | |
| #PSA_ERROR_CORRUPTION_DETECTED | |
| #PSA_ERROR_STORAGE_FAILURE | |
| #PSA_ERROR_INSUFFICIENT_ENTROPY | |
| #PSA_ERROR_BAD_STATE | The library has not been previously initialized by psa_crypto_init(). It is implementation-dependent whether a failure to initialize results in this error code. |
| psa_status_t psa_sign_hash | ( | psa_key_id_t | key, |
| psa_algorithm_t | alg, | ||
| const uint8_t * | hash, | ||
| size_t | hash_length, | ||
| uint8_t * | signature, | ||
| size_t | signature_size, | ||
| size_t * | signature_length | ||
| ) |
Sign a hash or short message with a private key.
Note that to perform a hash-and-sign signature algorithm, you must first calculate the hash by calling psa_hash_setup(), psa_hash_update() and psa_hash_finish(), or alternatively by calling psa_hash_compute(). Then pass the resulting hash as the hash parameter to this function. You can use #PSA_ALG_SIGN_GET_HASH(alg) to determine the hash algorithm to use.
| key | Identifier of the key to use for the operation. It must be an asymmetric key pair. The key must allow the usage #PSA_KEY_USAGE_SIGN_HASH. | |
| alg | A signature algorithm (PSA_ALG_XXX value such that #PSA_ALG_IS_SIGN_HASH(alg) is true), that is compatible with the type of key. For ECDSA, the digest length must match or exceed the curve length in security strength. This means the lengths will be the same in all cases except for SHA-512 with a 521-bit curve. | |
| [in] | hash | The hash or message to sign. |
| hash_length | Size of the hash buffer in bytes. | |
| [out] | signature | Buffer where the signature is to be written. |
| signature_size | Size of the signature buffer in bytes. | |
| [out] | signature_length | On success, the number of bytes that make up the returned signature value. |
| #PSA_SUCCESS | |
| #PSA_ERROR_INVALID_HANDLE | |
| #PSA_ERROR_NOT_PERMITTED | |
| #PSA_ERROR_BUFFER_TOO_SMALL | The size of the signature buffer is too small. You can determine a sufficient buffer size by calling #PSA_SIGN_OUTPUT_SIZE(key_type, key_bits, alg) where key_type and key_bits are the type and bit-size respectively of key. |
| #PSA_ERROR_NOT_SUPPORTED | |
| #PSA_ERROR_INVALID_ARGUMENT | |
| #PSA_ERROR_INSUFFICIENT_MEMORY | |
| #PSA_ERROR_COMMUNICATION_FAILURE | |
| #PSA_ERROR_HARDWARE_FAILURE | |
| #PSA_ERROR_CORRUPTION_DETECTED | |
| #PSA_ERROR_STORAGE_FAILURE | |
| #PSA_ERROR_INSUFFICIENT_ENTROPY | |
| #PSA_ERROR_BAD_STATE | The library has not been previously initialized by psa_crypto_init(). It is implementation-dependent whether a failure to initialize results in this error code. |
| psa_status_t psa_sign_message | ( | psa_key_id_t | key, |
| psa_algorithm_t | alg, | ||
| const uint8_t * | input, | ||
| size_t | input_length, | ||
| uint8_t * | signature, | ||
| size_t | signature_size, | ||
| size_t * | signature_length | ||
| ) |
Sign a message with a private key. For hash-and-sign algorithms, this includes the hashing step.
alg) can be used to determine the hash algorithm to use.| [in] | key | Identifier of the key to use for the operation. It must be an asymmetric key pair. The key must allow the usage #PSA_KEY_USAGE_SIGN_MESSAGE. |
| [in] | alg | An asymmetric signature algorithm (PSA_ALG_XXX value such that #PSA_ALG_IS_SIGN_MESSAGE(alg) is true), that is compatible with the type of key. For ECDSA, the digest length must match or exceed the curve length in security strength, per FIPS 186-4 guidelines. This means the lengths will be the same in all cases except for SHA-512 with a 521-bit curve. |
| [in] | input | The input message to sign. |
| [in] | input_length | Size of the input buffer in bytes. |
| [out] | signature | Buffer where the signature is to be written. |
| [in] | signature_size | Size of the signature buffer in bytes. This must be appropriate for the selected algorithm and key:
|
| [out] | signature_length | On success, the number of bytes that make up the returned signature value. |
| #PSA_SUCCESS | |
| #PSA_ERROR_INVALID_HANDLE | |
| #PSA_ERROR_NOT_PERMITTED | The key does not have the #PSA_KEY_USAGE_SIGN_MESSAGE flag, or it does not permit the requested algorithm. |
| #PSA_ERROR_BUFFER_TOO_SMALL | The size of the signature buffer is too small. You can determine a sufficient buffer size by calling #PSA_SIGN_OUTPUT_SIZE(key_type, key_bits, alg) where key_type and key_bits are the type and bit-size respectively of key. |
| #PSA_ERROR_NOT_SUPPORTED | |
| #PSA_ERROR_INVALID_ARGUMENT | |
| #PSA_ERROR_INSUFFICIENT_MEMORY | |
| #PSA_ERROR_COMMUNICATION_FAILURE | |
| #PSA_ERROR_HARDWARE_FAILURE | |
| #PSA_ERROR_CORRUPTION_DETECTED | |
| #PSA_ERROR_STORAGE_FAILURE | |
| #PSA_ERROR_DATA_CORRUPT | |
| #PSA_ERROR_DATA_INVALID | |
| #PSA_ERROR_INSUFFICIENT_ENTROPY | |
| #PSA_ERROR_BAD_STATE | The library has not been previously initialized by psa_crypto_init(). It is implementation-dependent whether a failure to initialize results in this error code. |
| psa_status_t psa_verify_hash | ( | psa_key_id_t | key, |
| psa_algorithm_t | alg, | ||
| const uint8_t * | hash, | ||
| size_t | hash_length, | ||
| const uint8_t * | signature, | ||
| size_t | signature_length | ||
| ) |
Verify the signature of a hash or short message using a public key.
Note that to perform a hash-and-sign signature algorithm, you must first calculate the hash by calling psa_hash_setup(), psa_hash_update() and psa_hash_finish(), or alternatively by calling psa_hash_compute(). Then pass the resulting hash as the hash parameter to this function. You can use #PSA_ALG_SIGN_GET_HASH(alg) to determine the hash algorithm to use.
| key | Identifier of the key to use for the operation. It must be a public key or an asymmetric key pair. The key must allow the usage #PSA_KEY_USAGE_VERIFY_HASH. | |
| alg | A signature algorithm (PSA_ALG_XXX value such that #PSA_ALG_IS_SIGN_HASH(alg) is true), that is compatible with the type of key. For ECDSA, the digest length must match the curve length in security strength. This means the lengths will be the same in all cases except for SHA-512 with a 521-bit curve. | |
| [in] | hash | The hash or message whose signature is to be verified. |
| hash_length | Size of the hash buffer in bytes. | |
| [in] | signature | Buffer containing the signature to verify. |
| signature_length | Size of the signature buffer in bytes. |
| #PSA_SUCCESS | The signature is valid. |
| #PSA_ERROR_INVALID_HANDLE | |
| #PSA_ERROR_NOT_PERMITTED | |
| #PSA_ERROR_INVALID_SIGNATURE | The calculation was performed successfully, but the passed signature is not a valid signature. |
| #PSA_ERROR_NOT_SUPPORTED | |
| #PSA_ERROR_INVALID_ARGUMENT | |
| #PSA_ERROR_INSUFFICIENT_MEMORY | |
| #PSA_ERROR_COMMUNICATION_FAILURE | |
| #PSA_ERROR_HARDWARE_FAILURE | |
| #PSA_ERROR_CORRUPTION_DETECTED | |
| #PSA_ERROR_STORAGE_FAILURE | |
| #PSA_ERROR_BAD_STATE | The library has not been previously initialized by psa_crypto_init(). It is implementation-dependent whether a failure to initialize results in this error code. |
| psa_status_t psa_verify_message | ( | psa_key_id_t | key, |
| psa_algorithm_t | alg, | ||
| const uint8_t * | input, | ||
| size_t | input_length, | ||
| const uint8_t * | signature, | ||
| size_t | signature_length | ||
| ) |
Verify the signature of a message with a public key, using a hash-and-sign verification algorithm.
alg) can be used to determine the hash algorithm to use.| [in] | key | Identifier of the key to use for the operation. It must be a public key or an asymmetric key pair. The key must allow the usage #PSA_KEY_USAGE_VERIFY_MESSAGE. |
| [in] | alg | An asymmetric signature algorithm (PSA_ALG_XXX value such that #PSA_ALG_IS_SIGN_MESSAGE(alg) is true), that is compatible with the type of key. For ECDSA, the digest length must match or exceed the curve length in security strength. This means the lengths will be the same in all cases except for SHA-512 with a 521-bit curve. |
| [in] | input | The message whose signature is to be verified. |
| [in] | input_length | Size of the input buffer in bytes. |
| [out] | signature | Buffer containing the signature to verify. |
| [in] | signature_length | Size of the signature buffer in bytes. |
| #PSA_SUCCESS | |
| #PSA_ERROR_INVALID_HANDLE | |
| #PSA_ERROR_NOT_PERMITTED | The key does not have the #PSA_KEY_USAGE_SIGN_MESSAGE flag, or it does not permit the requested algorithm. |
| #PSA_ERROR_INVALID_SIGNATURE | The calculation was performed successfully, but the passed signature is not a valid signature. |
| #PSA_ERROR_NOT_SUPPORTED | |
| #PSA_ERROR_INVALID_ARGUMENT | |
| #PSA_ERROR_INSUFFICIENT_MEMORY | |
| #PSA_ERROR_COMMUNICATION_FAILURE | |
| #PSA_ERROR_HARDWARE_FAILURE | |
| #PSA_ERROR_CORRUPTION_DETECTED | |
| #PSA_ERROR_STORAGE_FAILURE | |
| #PSA_ERROR_DATA_CORRUPT | |
| #PSA_ERROR_DATA_INVALID | |
| #PSA_ERROR_BAD_STATE | The library has not been previously initialized by psa_crypto_init(). It is implementation-dependent whether a failure to initialize results in this error code. |
1.8.12