TI BLE5-Stack API Documentation  9.14.02
Data Fields
hciEvt_BLEPhyUpdateComplete_t Struct Reference

LE Phy Update Complete Event. More...

Data Fields

uint8 BLEEventCode
 BLE Event Code. More...
 
uint16 connHandle
 connection handle More...
 
event_hdr_t hdr
 osal event header More...
 
uint8 rxPhy
 RX PHY. More...
 
uint8 status
 status of event More...
 
uint8 txPhy
 TX PHY. More...
 

Detailed Description

LE Phy Update Complete Event.

Field Documentation

§ BLEEventCode

uint8 BLEEventCode

BLE Event Code.

§ connHandle

uint16 connHandle

connection handle

§ hdr

osal event header

§ rxPhy

uint8 rxPhy

RX PHY.

§ status

uint8 status

status of event

§ txPhy

uint8 txPhy

TX PHY.


The documentation for this struct was generated from the following file:
© Copyright 1995-2026, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale