![]() |
![]() |
|
TI BLE5-Stack API Documentation
9.14.02
|
LE Periodic Advertising Sync Established event. More...
Data Fields | |
| uint8 | address [B_ADDR_LEN] |
| Peer address. More... | |
| uint8 | addrType |
| Peer address type. More... | |
| uint8 | BLEEventCode |
| BLE Event Code. More... | |
| uint8 | clockAccuracy |
| Peer Clock Accuracy. More... | |
| event_hdr_t | hdr |
| osal event header More... | |
| uint16 | periodicInterval |
| Periodic interval. More... | |
| uint8 | phy |
| Peer PHY. More... | |
| uint8 | sid |
| Peer SID. More... | |
| uint8 | status |
| status of event More... | |
| uint16 | syncHandle |
| sync handle More... | |
LE Periodic Advertising Sync Established event.
| uint8 address[B_ADDR_LEN] |
Peer address.
| uint8 addrType |
Peer address type.
| uint8 BLEEventCode |
BLE Event Code.
| uint8 clockAccuracy |
Peer Clock Accuracy.
| event_hdr_t hdr |
osal event header
| uint16 periodicInterval |
Periodic interval.
| uint8 phy |
Peer PHY.
| uint8 sid |
Peer SID.
| uint8 status |
status of event
| uint16 syncHandle |
sync handle