![]() |
![]() |
|
TI BLE5-Stack API Documentation
9.14.02
|
LE Periodic Advertising Report event. More...
Data Fields | |
| uint8 | BLEEventCode |
| BLE Event Code. More... | |
| uint8 | cteType |
| CTE type received. More... | |
| uint8 * | data |
| Periodic data received from peer. More... | |
| uint8 | dataLen |
| Periodic data length. More... | |
| uint8 | dataStatus |
| Periodic data status. More... | |
| event_hdr_t | hdr |
| osal event header More... | |
| int8 | rssi |
| RSSI of the received packet. More... | |
| uint16 | syncHandle |
| sync handle More... | |
| int8 | txPower |
| Tx Power information. More... | |
LE Periodic Advertising Report event.
| uint8 BLEEventCode |
BLE Event Code.
| uint8 cteType |
CTE type received.
| uint8* data |
Periodic data received from peer.
| uint8 dataLen |
Periodic data length.
| uint8 dataStatus |
Periodic data status.
| event_hdr_t hdr |
osal event header
| int8 rssi |
RSSI of the received packet.
| uint16 syncHandle |
sync handle
| int8 txPower |
Tx Power information.