![]() |
![]() |
|
TI BLE5-Stack API Documentation
9.14.02
|
Host Handover Serving Node Configuration parameters. More...
Data Fields | |
| uint16_t | connHandle |
| Connection handle. More... | |
| uint32_t | handoverDataSize |
| The stack handover data size. More... | |
| uint8_t | handoverSnMode |
| 0 - Terminate the connection immediately on the serving node side, 1 - wait for the candidate response More... | |
| uint16_t | maxGattHandle |
| Maximum GATT handle. More... | |
| uint16_t | minGattHandle |
| Minimum GATT handle. More... | |
| uint8_t * | pHandoverData |
| Pointer to the buffer the application allocated. More... | |
| uint32_t | rfu |
| Reserved for future use. More... | |
Host Handover Serving Node Configuration parameters.
| uint16_t connHandle |
Connection handle.
| uint32_t handoverDataSize |
The stack handover data size.
| uint8_t handoverSnMode |
0 - Terminate the connection immediately on the serving node side, 1 - wait for the candidate response
| uint16_t maxGattHandle |
Maximum GATT handle.
| uint16_t minGattHandle |
Minimum GATT handle.
| uint8_t* pHandoverData |
Pointer to the buffer the application allocated.
| uint32_t rfu |
Reserved for future use.