TI BLE5-Stack API Documentation  9.14.02
Data Fields
gapPairingReqEvent_t Struct Reference

Data Fields

uint16_t connectionHandle
 connection Handle More...
 
osal_event_hdr_t hdr
 GAP_MSG_EVENT and status More...
 
uint8_t opcode
 GAP_PAIRING_REQ_EVENT More...
 
gapPairingReq_t pairReq
 The Pairing Request fields received. More...
 

Detailed Description

GAP_PAIRING_REQ_EVENT message format.

This message is sent when an unexpected Pairing Request is received and pairing must be initiated with GAP_Authenticate using the pairReq field received here

Note
This message should only be sent to peripheral devices.

This event will be consumed by the gapbondmgr if it exists.

Field Documentation

§ connectionHandle

uint16_t connectionHandle

connection Handle

§ hdr

GAP_MSG_EVENT and status

§ opcode

uint8_t opcode

§ pairReq

gapPairingReq_t pairReq

The Pairing Request fields received.


The documentation for this struct was generated from the following file:
© Copyright 1995-2026, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale