TI BLE5-Stack API Documentation  9.14.02
Data Fields
attWriteReq_t Struct Reference

Write Request format. More...

Data Fields

uint8 cmd
 Command Flag. More...
 
uint16 handle
 Handle of the attribute to be written (must be first field) More...
 
uint16 len
 Length of value. More...
 
uint8 * pValue
 Value of the attribute to be written (0 to ATT_MTU_SIZE-3) More...
 
uint8 sig
 Authentication Signature status (not included (0), valid (1), invalid (2)) More...
 

Detailed Description

Write Request format.

for method ATT_WRITE_REQ

Field Documentation

§ cmd

uint8 cmd

Command Flag.

§ handle

uint16 handle

Handle of the attribute to be written (must be first field)

§ len

uint16 len

Length of value.

§ pValue

uint8* pValue

Value of the attribute to be written (0 to ATT_MTU_SIZE-3)

§ sig

uint8 sig

Authentication Signature status (not included (0), valid (1), invalid (2))


The documentation for this struct was generated from the following file:
© Copyright 1995-2026, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale