TI BLE5-Stack API Documentation  9.14.02
Data Fields
attReadMultiReq_t Struct Reference

Read Multiple Request format. More...

Data Fields

uint16 numHandles
 Number of attribute handles. More...
 
uint8 * pHandles
 Set of two or more attribute handles (4 to ATT_MTU_SIZE-1) - must be first field. More...
 

Detailed Description

Read Multiple Request format.

for method ATT_READ_MULTI_REQ

Field Documentation

§ numHandles

uint16 numHandles

Number of attribute handles.

§ pHandles

uint8* pHandles

Set of two or more attribute handles (4 to ATT_MTU_SIZE-1) - must be first field.


The documentation for this struct was generated from the following file:
© Copyright 1995-2026, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale