TI BLE5-Stack API Documentation  9.14.02
Data Fields
GapAdv_setTerm_t Struct Reference

Data type returned with GAP_EVT_ADV_SET_TERMINATED event. More...

Data Fields

uint16 connHandle
 Connection handle that ended advertising. More...
 
uint8 handle
 Advertising handle. More...
 
uint8 numCompAdvEvts
 Number of completed advertising events. More...
 
uint8 status
 Termination status. More...
 

Detailed Description

Data type returned with GAP_EVT_ADV_SET_TERMINATED event.

Field Documentation

§ connHandle

uint16 connHandle

Connection handle that ended advertising.

§ handle

uint8 handle

Advertising handle.

§ numCompAdvEvts

uint8 numCompAdvEvts

Number of completed advertising events.

§ status

uint8 status

Termination status.


The documentation for this struct was generated from the following file:
© Copyright 1995-2026, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale