TI BLE5-Stack API Documentation  9.14.02
Data Fields
GapAdv_scanReqReceived_t Struct Reference

Data type returned with GAP_EVT_SCAN_REQ_RECEIVED event. More...

Data Fields

uint8 channel
 Channel when the scan req was received. More...
 
uint8 handle
 Advertising handle. More...
 
int8 rssi
 RSSI of the scan req. More...
 
uint8 scanAddr [B_ADDR_LEN]
 Address of scanning device. More...
 
uint8 scanAddrType
 Address type of scanning device. More...
 

Detailed Description

Data type returned with GAP_EVT_SCAN_REQ_RECEIVED event.

Field Documentation

§ channel

uint8 channel

Channel when the scan req was received.

§ handle

uint8 handle

Advertising handle.

§ rssi

int8 rssi

RSSI of the scan req.

§ scanAddr

uint8 scanAddr[B_ADDR_LEN]

Address of scanning device.

§ scanAddrType

uint8 scanAddrType

Address type of scanning device.


The documentation for this struct was generated from the following file:
© Copyright 1995-2026, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale