![]() |
![]() |
|
TI BLE5-Stack API Documentation
9.14.02
|
Data Fields | |
| uint8_t | ch3CJump |
| Channel 3C jump. More... | |
| uint8_t | ch3cShape |
| Channel 3C shape. More... | |
| csChm_t | channelMap |
| Channel map csChm_t. More... | |
| uint8_t | chMRepetition |
| Channel map repetition. More... | |
| uint8_t | chSel |
| Channel selection algorithm to be used CS_Chan_Sel_Alg. More... | |
| uint8_t | configID |
| Configuration ID. More... | |
| uint16_t | connHandle |
| Connection handle. More... | |
| uint8_t | createContext |
| Create context flag. More... | |
| uint8_t | csSyncPhy |
| CS sync PHY CS_Sync_Phy_Supported. More... | |
| uint8_t | mainMode |
| Main mode CS_Mode. More... | |
| uint8_t | mainModeMaxSteps |
| Maximum steps for main mode. More... | |
| uint8_t | mainModeMinSteps |
| Minimum steps for main mode. More... | |
| uint8_t | mainModeRepetition |
| Main mode repetition. More... | |
| uint8_t | modeZeroSteps |
| Steps for mode zero. More... | |
| uint8_t | role |
| Role CS_Role. More... | |
| uint8_t | rttType |
| RTT type CS_RTT_Type. More... | |
| uint8_t | subMode |
| Sub mode CS_Mode. More... | |
| uint8_t ch3CJump |
Channel 3C jump.
| uint8_t ch3cShape |
Channel 3C shape.
| csChm_t channelMap |
Channel map csChm_t.
| uint8_t chMRepetition |
Channel map repetition.
| uint8_t chSel |
Channel selection algorithm to be used CS_Chan_Sel_Alg.
| uint8_t configID |
Configuration ID.
| uint16_t connHandle |
Connection handle.
| uint8_t createContext |
Create context flag.
| uint8_t csSyncPhy |
CS sync PHY CS_Sync_Phy_Supported.
| uint8_t mainMode |
Main mode CS_Mode.
| uint8_t mainModeMaxSteps |
Maximum steps for main mode.
| uint8_t mainModeMinSteps |
Minimum steps for main mode.
| uint8_t mainModeRepetition |
Main mode repetition.
| uint8_t modeZeroSteps |
Steps for mode zero.
| uint8_t role |
Role CS_Role.
| uint8_t rttType |
RTT type CS_RTT_Type.
| uint8_t subMode |
Sub mode CS_Mode.