TI BLE5-Stack API Documentation  9.14.02
Data Fields
BLEAppUtil_ScanEventData_t Struct Reference

BLEAppUtil Scan Event Data Structure. More...

Data Fields

uint32_t * arg
 custom application argument that can be return through this callback More...
 
uint32_t event
 see BLEAppUtil_GAPScanEventMaskFlags_e More...
 
GapScan_data_tpBuf
 data potentially accompanying event More...
 

Detailed Description

BLEAppUtil Scan Event Data Structure.

Used to store the data of scan event

Field Documentation

§ arg

uint32_t* arg

custom application argument that can be return through this callback

§ event

uint32_t event

§ pBuf

data potentially accompanying event


The documentation for this struct was generated from the following file:
© Copyright 1995-2026, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale