![]() |
![]() |
|
TI BLE5-Stack API Documentation
9.14.02
|
Phy Preference on the current connection. Should be created by the application and passed to BLEAppUtil_setConnPhy. More...
Data Fields | |
| uint8 | allPhys |
| Host preference on how to handle txPhy and rxPhy. More... | |
| uint16 | connHandle |
| Connection handle. More... | |
| uint16 | phyOpts |
| Bit field of Host preferred PHY options. More... | |
| uint8 | rxPhy |
| Bit field of Host preferred Rx PHY. More... | |
| uint8 | txPhy |
| Bit field of Host preferred Tx PHY. More... | |
Phy Preference on the current connection. Should be created by the application and passed to BLEAppUtil_setConnPhy.
| uint8 allPhys |
Host preference on how to handle txPhy and rxPhy.
| uint16 connHandle |
Connection handle.
| uint16 phyOpts |
Bit field of Host preferred PHY options.
| uint8 rxPhy |
Bit field of Host preferred Rx PHY.
| uint8 txPhy |
Bit field of Host preferred Tx PHY.