![]() |
![]() |
|
TI BLE5-Stack API Documentation
9.14.02
|
Macros | |
| #define | L2CAP_TERM_BY_PEER_PSM 0x0002 |
| Channel terminated by peer PSM. More... | |
| #define | L2CAP_TERM_BY_PSM 0x0001 |
| Channel terminated by local PSM. More... | |
| #define | L2CAP_TERM_LINK_DOWN 0x0000 |
| Physical link gone down. More... | |
| #define | L2CAP_TERM_MAX_CREDIT_EXCEED 0x0003 |
| Credit count exceeded 65535. More... | |
| #define | L2CAP_TERM_MEM_ALLOC_ERROR 0x0009 |
| Memory allocation error occurred. More... | |
| #define | L2CAP_TERM_PSM_MTU_EXCEED 0x0005 |
| Total length of payload received exceeded local PSM's MTU. More... | |
| #define | L2CAP_TERM_RX_ERROR 0x0007 |
| LE-frame was received with error. More... | |
| #define | L2CAP_TERM_RX_PKT_NO_CREDIT 0x0006 |
| LE-frame was received from peer device that has a credit of count zero. More... | |
| #define | L2CAP_TERM_SDU_LEN_EXCEED 0x0004 |
| Total length of payload received exceeded SDU length specified in first LE-frame of SDU. More... | |
| #define | L2CAP_TERM_TX_ERROR 0x0008 |
| Error happened while trying to send LE-frame. More... | |
| #define L2CAP_TERM_BY_PEER_PSM 0x0002 |
Channel terminated by peer PSM.
| #define L2CAP_TERM_BY_PSM 0x0001 |
Channel terminated by local PSM.
| #define L2CAP_TERM_LINK_DOWN 0x0000 |
Physical link gone down.
| #define L2CAP_TERM_MAX_CREDIT_EXCEED 0x0003 |
Credit count exceeded 65535.
| #define L2CAP_TERM_MEM_ALLOC_ERROR 0x0009 |
Memory allocation error occurred.
| #define L2CAP_TERM_PSM_MTU_EXCEED 0x0005 |
Total length of payload received exceeded local PSM's MTU.
| #define L2CAP_TERM_RX_ERROR 0x0007 |
LE-frame was received with error.
| #define L2CAP_TERM_RX_PKT_NO_CREDIT 0x0006 |
LE-frame was received from peer device that has a credit of count zero.
| #define L2CAP_TERM_SDU_LEN_EXCEED 0x0004 |
Total length of payload received exceeded SDU length specified in first LE-frame of SDU.
| #define L2CAP_TERM_TX_ERROR 0x0008 |
Error happened while trying to send LE-frame.