TI BLE5-Stack API Documentation  9.14.02
Macros

Macros

#define ATT_MAX_MTU_SIZE   (255-L2CAP_HDR_SIZE)
 Maximum ATT MTU size. More...
 
#define ATT_MTU_SIZE   L2CAP_MTU_SIZE
 Minimum ATT MTU size. More...
 

Detailed Description

The Exchanging MTU Size is defined as the maximum size of any packet transmitted between a client and a server. A higher layer specification defines the default ATT MTU value. The ATT MTU value should be within the range 23 to 251 inclusive. Refer to ble_user_config.h for the device-specific maximum MTU value.

Macro Definition Documentation

§ ATT_MAX_MTU_SIZE

#define ATT_MAX_MTU_SIZE   (255-L2CAP_HDR_SIZE)

Maximum ATT MTU size.

§ ATT_MTU_SIZE

#define ATT_MTU_SIZE   L2CAP_MTU_SIZE

Minimum ATT MTU size.

© Copyright 1995-2026, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale