22 #ifndef GAP_ADVERTISER_H 23 #define GAP_ADVERTISER_H 52 #define GAPADV_PARAMS_LEGACY_SCANN_CONN { \ 54 .eventProps = GAP_ADV_PROP_CONNECTABLE | GAP_ADV_PROP_SCANNABLE | \ 55 GAP_ADV_PROP_LEGACY, \ 58 .primChanMap = GAP_ADV_CHAN_ALL, \ 59 .peerAddrType = PEER_ADDRTYPE_PUBLIC_OR_PUBLIC_ID, \ 60 .peerAddr = { 0xaa, 0xaa, 0xaa, 0xaa, 0xaa, 0xaa }, \ 61 .filterPolicy = GAP_ADV_AL_POLICY_ANY_REQ, \ 62 .txPower = GAP_ADV_TX_POWER_NO_PREFERENCE, \ 63 .primPhy = GAP_ADV_PRIM_PHY_1_MBPS, \ 64 .secPhy = GAP_ADV_SEC_PHY_1_MBPS, \ 70 #define GAPADV_PARAMS_AE_LONG_RANGE_CONN { \ 72 .eventProps = GAP_ADV_PROP_CONNECTABLE, \ 75 .primChanMap = GAP_ADV_CHAN_ALL, \ 76 .peerAddrType = PEER_ADDRTYPE_PUBLIC_OR_PUBLIC_ID, \ 77 .peerAddr = { 0xaa, 0xaa, 0xaa, 0xaa, 0xaa, 0xaa }, \ 78 .filterPolicy = GAP_ADV_AL_POLICY_ANY_REQ, \ 79 .txPower = GAP_ADV_TX_POWER_NO_PREFERENCE, \ 80 .primPhy = GAP_ADV_PRIM_PHY_CODED_S2, \ 81 .secPhy = GAP_ADV_SEC_PHY_CODED_S2, \ 87 #define GAPADV_PARAMS_AE_NC_NS { \ 91 .primChanMap = GAP_ADV_CHAN_ALL, \ 92 .peerAddrType = PEER_ADDRTYPE_PUBLIC_OR_PUBLIC_ID, \ 93 .peerAddr = { 0xaa, 0xaa, 0xaa, 0xaa, 0xaa, 0xaa }, \ 94 .filterPolicy = GAP_ADV_AL_POLICY_ANY_REQ, \ 95 .txPower = GAP_ADV_TX_POWER_NO_PREFERENCE, \ 96 .primPhy = GAP_ADV_PRIM_PHY_1_MBPS, \ 97 .secPhy = GAP_ADV_SEC_PHY_1_MBPS, \ 341 #define GAP_ADV_INVALID_HANDLE 0xFF 432 #define GAP_ADV_TX_POWER_NO_PREFERENCE 127 497 GAP_ADV_EVT_MASK_RESERVED =
BV(15)
506 #define GAPADV_PERIODIC_ADV_INTERVAL_MIN 0x0006 508 #define GAPADV_PERIODIC_ADV_INTERVAL_MAX 0xFFFF 510 #define GAPADV_PERIODIC_ADV_ENABLE_TX_POWER 0x0040 512 #define GAPADV_PERIODIC_ADV_DISABLE_TX_POWER 0x0000 514 #define GAPADV_PERIODIC_ADV_DATA_INTERMIDIATE_FRAG 0x00 516 #define GAPADV_PERIODIC_ADV_DATA_FIRST_FRAG 0x01 518 #define GAPADV_PERIODIC_ADV_DATA_LAST_FRAG 0x02 520 #define GAPADV_PERIODIC_ADV_DATA_COMPLETE 0x03 522 #define GAPADV_PERIODIC_ADV_MAX_DATA_LEN 252 597 uint16 periodicAdvIntervalMin;
598 uint16 periodicAdvIntervalMax;
599 uint16 periodicAdvProp;
600 } GapAdv_periodicAdvParams_t;
614 } GapAdv_periodicAdvData_t;
621 } GapAdv_periodicAdvEvt_t;
630 } GapAdv_dataUpdateEvent_t;
636 } GapAv_setAdvStatusDoneEvent_t;
695 GapAdv_freeBufferOptions_t freeOptions);
732 GapAdv_enableOptions_t enableOptions,
733 uint16 durationOrMaxEvents);
814 void *pValue, uint8_t *pLen);
834 uint16 *pLen, uint8 **ppBuf);
895 GapAdv_freeBufferOptions_t freeOptions);
942 uint16 len, uint8 *pBuf);
1065 uint8_t GapAdv_SetPeriodicAdvParams( uint8 advHandle,
1066 GapAdv_periodicAdvParams_t *periodicAdvParams );
1084 bStatus_t GapAdv_SetPeriodicAdvData( uint8 advHandle,
1085 GapAdv_periodicAdvData_t *periodicAdvData );
1103 bStatus_t GapAdv_SetPeriodicAdvEnable( uint8 enable,
Omit advertiser's address from PDU's.
Definition: gap_advertiser.h:352
uint32_t primIntMax
GAP_ADV_PARAM_PRIMARY_INTERVAL_MAX
Definition: gap_advertiser.h:549
This API allows the software components in the Z-Stack to be written independently of the specifics o...
All Channels.
Definition: gap_advertiser.h:402
GAP_Peer_Addr_Types_t
Address types used for specifying peer address type.
Definition: gap.h:745
coded-s2
Definition: gap_advertiser.h:439
Channels 37 & 39.
Definition: gap_advertiser.h:398
bStatus_t GapAdv_setParam(uint8 handle, GapAdv_ParamId_t paramID, void *pValue)
bStatus_t GapAdv_getParam(uint8 handle, GapAdv_ParamId_t paramID, void *pValue, uint8_t *pLen)
Definition: gap_advertiser.h:294
uint32_t primIntMin
GAP_ADV_PARAM_PRIMARY_INTERVAL_MIN
Definition: gap_advertiser.h:548
bStatus_t GapAdv_prepareLoadByHandle(uint8 handle, GapAdv_freeBufferOptions_t freeOptions)
GapAdv_freeBufferOptions_t
Possible free options for Gap Advertiser API's.
Definition: gap_advertiser.h:365
Definition: gap_advertiser.h:487
1 mbps
Definition: gap_advertiser.h:437
Definition: gap_advertiser.h:226
Definition: gap_advertiser.h:328
bStatus_t GapAdv_loadByHandle(uint8 handle, GapAdv_dataTypes_t dataType, uint16 len, uint8 *pBuf)
Definition: gap_advertiser.h:353
Directed advertising.
Definition: gap_advertiser.h:349
bStatus_t GapAdv_abortLoad(void)
bStatus_t GapAdv_setVirtualAdvAddr(uint8 advHandle, uint8 *bdAddr)
Definition: gap_advertiser.h:475
bStatus_t GapAdv_enable(uint8 handle, GapAdv_enableOptions_t enableOptions, uint16 durationOrMaxEvents)
Data type returned with GAP_EVT_ADV_DATA_TRUNCATED event.
Definition: gap_advertiser.h:582
int8 rssi
RSSI of the scan req.
Definition: gap_advertiser.h:578
Scannable advertising.
Definition: gap_advertiser.h:348
uint16_t eventProps
GAP_ADV_PARAM_PROPS
Definition: gap_advertiser.h:547
Free the scan response data.
Definition: gap_advertiser.h:369
uint8 channel
Channel when the scan req was received.
Definition: gap_advertiser.h:577
GapAdv_enableOptions_t
Enable options for GapAdv_enable.
Definition: gap_advertiser.h:373
Definition: gap_advertiser.h:463
GapAdv_ParamId_t
Definition: gap_advertiser.h:162
Definition: gap_advertiser.h:414
1 mbps
Definition: gap_advertiser.h:445
uint8 handle
Advertising handle.
Definition: gap_advertiser.h:565
Definition: gap_advertiser.h:311
Don't free anything.
Definition: gap_advertiser.h:367
Definition: gap_advertiser.h:280
Definition: gap_advertiser.h:419
Channels 38 & 39.
Definition: gap_advertiser.h:400
bStatus_t GapAdv_disable(uint8 handle)
Disable an active advertising set.
Definition: gap_advertiser.h:424
void(* pfnGapCB_t)(uint32_t event, void *pBuf, uintptr_t arg)
Definition: gap.h:1358
uint8 handle
Advertising handle.
Definition: gap_advertiser.h:584
Definition: gap_advertiser.h:235
GapAdv_secondaryPHY_t secPhy
GAP_ADV_PARAM_SECONDARY_PHY
Definition: gap_advertiser.h:556
2 mbps
Definition: gap_advertiser.h:446
Scan response data.
Definition: gap_advertiser.h:361
bStatus_t GapAdv_setEventMask(uint8 handle, GapAdv_eventMaskFlags_t mask)
GapAdv_secondaryPHY_t
Gap Advertiser Options for advertising on the secondary PHY.
Definition: gap_advertiser.h:443
bStatus_t GapAdv_create(pfnGapCB_t *cb, GapAdv_params_t *advParam, uint8 *advHandle)
#define BV(n)
Definition: comdef.h:136
Definition: gap_advertiser.h:483
Definition: gap_advertiser.h:256
GapAdv_advChannels_t
GAP Advertiser Defines for Advertiser Channels.
Definition: gap_advertiser.h:391
Definition: gap_advertiser.h:196
Channels 37 & 38.
Definition: gap_advertiser.h:396
GAP_Peer_Addr_Types_t peerAddrType
GAP_ADV_PARAM_PEER_ADDRESS_TYPE
Definition: gap_advertiser.h:551
GapAdv_eventMaskFlags_t
Definition: gap_advertiser.h:458
Advertising data.
Definition: gap_advertiser.h:360
GapAdv_primaryPHY_t
Gap Advertiser Options for advertising on the primary PHY.
Definition: gap_advertiser.h:435
Definition: gap_advertiser.h:387
Type definitions and macros for BLE stack.
Channel 37.
Definition: gap_advertiser.h:393
Definition: gap_advertiser.h:182
Connectable advertising.
Definition: gap_advertiser.h:347
Free the advertising data.
Definition: gap_advertiser.h:368
Definition: gap_advertiser.h:383
bStatus_t GapAdv_getBuffer(uint8 handle, GapAdv_dataTypes_t dataType, uint16 *pLen, uint8 **ppBuf)
coded-s2
Definition: gap_advertiser.h:448
Definition: gap_advertiser.h:268
Definition: gap_advertiser.h:471
uint16 connHandle
Connection handle that ended advertising.
Definition: gap_advertiser.h:567
Generic Event Header.
Definition: bcomdef.h:223
Definition: gap_advertiser.h:467
coded-s8
Definition: gap_advertiser.h:447
GapAdv_filterPolicy_t filterPolicy
GAP_ADV_PARAM_FILTER_POLICY
Definition: gap_advertiser.h:553
GapAdv_advChannels_t primChanMap
GAP_ADV_PARAM_PRIMARY_CHANNEL_MAP
Definition: gap_advertiser.h:550
Use legacy advertising PDU's.
Definition: gap_advertiser.h:351
GapAdv_dataTypes_t
Gap Advertising Data Types.
Definition: gap_advertiser.h:358
Definition: gap_advertiser.h:379
uint8 scanAddrType
Address type of scanning device.
Definition: gap_advertiser.h:575
uint16 advDataLen
Definition: gap_advertiser.h:589
int8_t txPower
GAP_ADV_PARAM_TX_POWER
Definition: gap_advertiser.h:554
Data type returned with GAP_EVT_ADV_SET_TERMINATED event.
Definition: gap_advertiser.h:563
#define B_ADDR_LEN
Default Public and Random Address Length.
Definition: bcomdef.h:73
Definition: gap_advertiser.h:171
Definition: gap_advertiser.h:545
Definition: gap_advertiser.h:479
High Duty Cycle Directed Advertising.
Definition: gap_advertiser.h:350
Definition: gap_advertiser.h:217
GapAdv_filterPolicy_t
GAP Advertiser Accept List Policy.
Definition: gap_advertiser.h:408
bStatus_t GapAdv_prepareLoadByBuffer(uint8 *pBuf, bool freeOldData)
bStatus_t GapAdv_loadByBuffer(uint16 len, uint8 *pBuf)
Definition: gap_advertiser.h:428
uint8_t zeroDelay
GAP_ADV_PARAM_ZERODELAY
Definition: gap_advertiser.h:558
Channel 39.
Definition: gap_advertiser.h:395
bStatus_t GapAdv_destroy(uint8 handle, GapAdv_freeBufferOptions_t freeOptions)
uint8 handle
Advertising handle.
Definition: gap_advertiser.h:574
GapAdv_eventProps_t
GAP Advertising Event Param Properties.
Definition: gap_advertiser.h:345
coded-s8
Definition: gap_advertiser.h:438
Data type returned with GAP_EVT_SCAN_REQ_RECEIVED event.
Definition: gap_advertiser.h:572
uint8_t bStatus_t
BLE Generic Status return.
Definition: bcomdef.h:220
Channel 38.
Definition: gap_advertiser.h:394
GapAdv_primaryPHY_t primPhy
GAP_ADV_PARAM_PRIMARY_PHY
Definition: gap_advertiser.h:555
uint8_t sid
GAP_ADV_PARAM_SID
Definition: gap_advertiser.h:557
uint8 status
Termination status.
Definition: gap_advertiser.h:566
uint8 numCompAdvEvts
Number of completed advertising events.
Definition: gap_advertiser.h:568
Definition: gap_advertiser.h:208
uint8 availAdvDataLen
How many bytes of the advertising data were sent.
Definition: gap_advertiser.h:585