![]() |
![]() |
|
TI BLE5-Stack API Documentation
9.14.02
|
GAP layer interface.
Go to the source code of this file.
Data Structures | |
| struct | Gap_ConnEventRpt_t |
| struct | gapAuthCompleteEvent_t |
| struct | gapAuthParams_t |
| struct | gapBondCompleteEvent_t |
| struct | gapBondLostEvent_t |
| struct | gapBondMgrCBs_t |
| Callback Registration Structure. More... | |
| struct | gapDeviceInitDoneEvent_t |
| struct | gapEstLinkReqEvent_t |
| struct | gapEventHdr_t |
| GAP event header format. More... | |
| struct | gapLinkUpdateEvent_t |
| struct | gapPairingReq_t |
| struct | gapPairingReqEvent_t |
| struct | gapPasskeyNeededEvent_t |
| struct | gapPeriConnectParams_t |
| struct | gapPeripheralSecurityReqEvent_t |
| struct | gapSignUpdateEvent_t |
| struct | gapTerminateLinkEvent_t |
| struct | gapUpdateLinkParamReq_t |
| struct | gapUpdateLinkParamReqEvent_t |
| GAP_UPDATE_LINK_PARAM_REQ_EVENT message format. More... | |
| struct | gapUpdateLinkParamReqReply_t |
Macros | |
| #define | GAP_ADTYPE_128BIT_COMPLETE 0x07 |
| Service: Complete list of 128-bit UUIDs. More... | |
| #define | GAP_ADTYPE_128BIT_MORE 0x06 |
| Service: More 128-bit UUIDs available. More... | |
| #define | GAP_ADTYPE_16BIT_COMPLETE 0x03 |
| Service: Complete list of 16-bit UUIDs. More... | |
| #define | GAP_ADTYPE_16BIT_MORE 0x02 |
| Service: More 16-bit UUIDs available. More... | |
| #define | GAP_ADTYPE_32BIT_COMPLETE 0x05 |
| Service: Complete list of 32-bit UUIDs. More... | |
| #define | GAP_ADTYPE_32BIT_MORE 0x04 |
| Service: More 32-bit UUIDs available. More... | |
| #define | GAP_ADTYPE_3D_INFO_DATA 0x3D |
| 3D Information Data More... | |
| #define | GAP_ADTYPE_ADV_INTERVAL 0x1A |
| Advertising Interval. More... | |
| #define | GAP_ADTYPE_APPEARANCE 0x19 |
| Appearance. More... | |
| #define | GAP_ADTYPE_FLAGS 0x01 |
| Gap Advertising Flags. More... | |
| #define | GAP_ADTYPE_FLAGS_BREDR_NOT_SUPPORTED 0x04 |
| Discovery Mode: BR/EDR Not Supported. More... | |
| #define | GAP_ADTYPE_FLAGS_GENERAL 0x02 |
| Discovery Mode: LE General Discoverable Mode. More... | |
| #define | GAP_ADTYPE_FLAGS_LIMITED 0x01 |
| Discovery Mode: LE Limited Discoverable Mode. More... | |
| #define | GAP_ADTYPE_LE_BD_ADDR 0x1B |
| LE Bluetooth Device Address. More... | |
| #define | GAP_ADTYPE_LE_ROLE 0x1C |
| LE Role. More... | |
| #define | GAP_ADTYPE_LOCAL_NAME_COMPLETE 0x09 |
| Complete local name. More... | |
| #define | GAP_ADTYPE_LOCAL_NAME_SHORT 0x08 |
| Shortened local name. More... | |
| #define | GAP_ADTYPE_MANUFACTURER_SPECIFIC 0xFF |
| #define | GAP_ADTYPE_OOB_CLASS_OF_DEVICE 0x0D |
| Simple Pairing OOB Tag: Class of device (3 octets) More... | |
| #define | GAP_ADTYPE_OOB_SIMPLE_PAIRING_HASHC 0x0E |
| Simple Pairing OOB Tag: Simple Pairing Hash C (16 octets) More... | |
| #define | GAP_ADTYPE_OOB_SIMPLE_PAIRING_RANDR 0x0F |
| Simple Pairing OOB Tag: Simple Pairing Randomizer R (16 octets) More... | |
| #define | GAP_ADTYPE_PERIPHERAL_CONN_INTERVAL_RANGE 0x12 |
| #define | GAP_ADTYPE_POWER_LEVEL 0x0A |
| TX Power Level: 0xXX: -127 to +127 dBm. More... | |
| #define | GAP_ADTYPE_PUBLIC_TARGET_ADDR 0x17 |
| Public Target Address. More... | |
| #define | GAP_ADTYPE_RANDOM_TARGET_ADDR 0x18 |
| Random Target Address. More... | |
| #define | GAP_ADTYPE_SERVICE_DATA 0x16 |
| Service Data - 16-bit UUID. More... | |
| #define | GAP_ADTYPE_SERVICE_DATA_128BIT 0x21 |
| Service Data - 128-bit UUID. More... | |
| #define | GAP_ADTYPE_SERVICE_DATA_32BIT 0x20 |
| Service Data - 32-bit UUID. More... | |
| #define | GAP_ADTYPE_SERVICES_LIST_128BIT 0x15 |
| Service Solicitation: list of 128-bit Service UUIDs. More... | |
| #define | GAP_ADTYPE_SERVICES_LIST_16BIT 0x14 |
| Service Solicitation: list of 16-bit Service UUIDs. More... | |
| #define | GAP_ADTYPE_SIGNED_DATA 0x13 |
| Signed Data field. More... | |
| #define | GAP_ADTYPE_SIMPLE_PAIRING_HASHC_256 0x1D |
| Simple Pairing Hash C-256. More... | |
| #define | GAP_ADTYPE_SIMPLE_PAIRING_RANDR_256 0x1E |
| Simple Pairing Randomizer R-256. More... | |
| #define | GAP_ADTYPE_SM_OOB_FLAG 0x11 |
| Security Manager OOB Flags. More... | |
| #define | GAP_ADTYPE_SM_TK 0x10 |
| Security Manager TK Value. More... | |
| #define | GAP_ADV_REMOVE_SET_EVENT 0x13 |
| Sent when an advertising set needs to be removed. This is an internal event. More... | |
| #define | GAP_ADV_SET_PERIODIC_ADV_DATA_EVENT 0x1A |
| Set periodic advertising data command complete event. More... | |
| #define | GAP_ADV_SET_PERIODIC_ADV_ENABLE_EVENT 0x1B |
| Set periodic advertising enable command complete event. More... | |
| #define | GAP_ADV_SET_PERIODIC_ADV_PARAMS_EVENT 0x19 |
| Set periodic advertising parameters command complete event. More... | |
| #define | GAP_APPEARE_GENERIC_BARCODE_SCANNER 0x02C0 |
| Generic Barcode Scanner. More... | |
| #define | GAP_APPEARE_GENERIC_BLOOD_PRESSURE 0x0380 |
| Generic Blood Pressure. More... | |
| #define | GAP_APPEARE_GENERIC_BP_ARM 0x0381 |
| Blood Pressure: Arm. More... | |
| #define | GAP_APPEARE_GENERIC_BP_WRIST 0x0382 |
| Blood Pressure: Wrist. More... | |
| #define | GAP_APPEARE_GENERIC_CLOCK 0x0100 |
| Generic Clock. More... | |
| #define | GAP_APPEARE_GENERIC_COMPUTER 0x0080 |
| Generic Computer. More... | |
| #define | GAP_APPEARE_GENERIC_DISPLAY 0x0140 |
| Generic Display. More... | |
| #define | GAP_APPEARE_GENERIC_EYE_GALSSES 0x01C0 |
| Generic Eye-glasses. More... | |
| #define | GAP_APPEARE_GENERIC_HID 0x03C0 |
| Generic Human Interface Device (HID) More... | |
| #define | GAP_APPEARE_GENERIC_HR_SENSOR 0x0340 |
| Generic Heart rate Sensor. More... | |
| #define | GAP_APPEARE_GENERIC_HRS_BELT 0x0341 |
| Heart Rate Sensor: Heart Rate Belt. More... | |
| #define | GAP_APPEARE_GENERIC_KEYRING 0x0240 |
| Generic Keyring. More... | |
| #define | GAP_APPEARE_GENERIC_MEDIA_PLAYER 0x0280 |
| Generic Media Player. More... | |
| #define | GAP_APPEARE_GENERIC_PHONE 0x0040 |
| Generic Phone. More... | |
| #define | GAP_APPEARE_GENERIC_RC 0x0180 |
| Generic Remote Control. More... | |
| #define | GAP_APPEARE_GENERIC_TAG 0x0200 |
| Generic Tag. More... | |
| #define | GAP_APPEARE_GENERIC_THERMO_EAR 0x0301 |
| Thermometer: Ear. More... | |
| #define | GAP_APPEARE_GENERIC_THERMOMETER 0x0300 |
| Generic Thermometer. More... | |
| #define | GAP_APPEARE_GENERIC_WATCH 0x00C0 |
| Generic Watch. More... | |
| #define | GAP_APPEARE_HID_BARCODE_SCANNER 0x03C8 |
| HID Barcode Scanner. More... | |
| #define | GAP_APPEARE_HID_DIGITAL_CARDREADER 0x03C6 |
| HID Card Reader. More... | |
| #define | GAP_APPEARE_HID_DIGITAL_PEN 0x03C7 |
| HID Digital Pen. More... | |
| #define | GAP_APPEARE_HID_DIGITIZER_TYABLET 0x03C5 |
| HID Digitizer Tablet. More... | |
| #define | GAP_APPEARE_HID_GAMEPAD 0x03C4 |
| HID Gamepad. More... | |
| #define | GAP_APPEARE_HID_JOYSTIC 0x03C3 |
| HID Joystick. More... | |
| #define | GAP_APPEARE_HID_KEYBOARD 0x03C1 |
| HID Keyboard. More... | |
| #define | GAP_APPEARE_HID_MOUSE 0x03C2 |
| HID Mouse. More... | |
| #define | GAP_APPEARE_UNKNOWN 0x0000 |
| Unknown. More... | |
| #define | GAP_APPEARE_WATCH_SPORTS 0x00C1 |
| Watch: Sports Watch. More... | |
| #define | GAP_AUTHENTICATION_COMPLETE_EVENT 0x0A |
| #define | GAP_AUTHENTICATION_FAILURE_EVT 0x10 |
| #define | GAP_BOND_COMPLETE_EVENT 0x0E |
| #define | GAP_BOND_LOST_EVENT 0x17 |
| #define | GAP_CONNECTING_CANCELLED_EVENT 0x15 |
| #define | GAP_DEVICE_INIT_DONE_EVENT 0x00 |
| #define | GAP_EVT_ADV_DATA_TRUNCATED (uint32_t)BV(6) |
| #define | GAP_EVT_ADV_END (uint32_t)BV(3) |
| #define | GAP_EVT_ADV_END_AFTER_DISABLE (uint32_t)BV(1) |
| #define | GAP_EVT_ADV_EVT_MASK |
| Mask for all advertising events. More... | |
| #define | GAP_EVT_ADV_REPORT (uint32_t)BV(22) |
| #define | GAP_EVT_ADV_REPORT_FULL (uint32_t)BV(23) |
| #define | GAP_EVT_ADV_SET_TERMINATED (uint32_t)BV(4) |
| #define | GAP_EVT_ADV_START (uint32_t)BV(2) |
| #define | GAP_EVT_ADV_START_AFTER_ENABLE (uint32_t)BV(0) |
| #define | GAP_EVT_INSUFFICIENT_MEMORY (uint32_t)BV(31) |
| A memory failure has occurred. More... | |
| #define | GAP_EVT_SCAN_DISABLED (uint32_t)BV(17) |
| #define | GAP_EVT_SCAN_DUR_ENDED (uint32_t)BV(19) |
| Scan duration has ended. More... | |
| #define | GAP_EVT_SCAN_ENABLED (uint32_t)BV(16) |
| Scanner has been enabled. More... | |
| #define | GAP_EVT_SCAN_EVT_MASK |
| Mask for all scan events. More... | |
| #define | GAP_EVT_SCAN_INT_ENDED (uint32_t)BV(20) |
| #define | GAP_EVT_SCAN_PRD_ENDED (uint32_t)BV(18) |
| #define | GAP_EVT_SCAN_REQ_RECEIVED (uint32_t)BV(5) |
| #define | GAP_EVT_SCAN_WND_ENDED (uint32_t)BV(21) |
| Scan window has ended. More... | |
| #define | GAP_IS_ADDR_RAND(pAddr) |
| #define | GAP_IS_ADDR_RPN(pAddr) |
| #define | GAP_IS_ADDR_RPR(pAddr) |
| #define | GAP_IS_ADDR_RS(pAddr) |
| #define | GAP_LINK_ESTABLISHED_EVENT 0x05 |
| #define | GAP_LINK_PARAM_UPDATE_EVENT 0x07 |
| #define | GAP_LINK_PARAM_UPDATE_REJECT_EVENT 0x18 |
| #define | GAP_LINK_TERMINATED_EVENT 0x06 |
| #define | GAP_PAIRING_REQ_EVENT 0x0F |
| #define | GAP_PASSKEY_NEEDED_EVENT 0x0B |
| #define | GAP_PERIPHERAL_REQUESTED_SECURITY_EVENT 0x0C |
| #define | GAP_PRIVACY_MODE_DEVICE 1 |
| Device Privacy Mode. More... | |
| #define | GAP_PRIVACY_MODE_NETWORK 0 |
| Network Privacy Mode. More... | |
| #define | GAP_PROFILE_BROADCASTER 0x01U |
| A device that sends advertising events only. More... | |
| #define | GAP_PROFILE_CENTRAL 0x08U |
| #define | GAP_PROFILE_OBSERVER 0x02U |
| A device that receives advertising events only. More... | |
| #define | GAP_PROFILE_PERIPHERAL 0x04U |
| #define | GAP_SCAN_ADD_DEVICE_ADV_LIST_EVENT 0x20 |
| Add device to period advertisers list command complete event. More... | |
| #define | GAP_SCAN_CLEAR_ADV_LIST_EVENT 0x23 |
| Clear period advertisers list command complete event. More... | |
| #define | GAP_SCAN_CREATE_SYNC_EVENT 0x1C |
| #define | GAP_SCAN_PERIODIC_ADV_REPORT_EVENT 0x26 |
| #define | GAP_SCAN_PERIODIC_ADV_SYNC_EST_EVENT 0x24 |
| #define | GAP_SCAN_PERIODIC_ADV_SYNC_LOST_EVENT 0x25 |
| #define | GAP_SCAN_PERIODIC_RECEIVE_EVENT 0x1F |
| Periodic advertising receive enable command complete event. More... | |
| #define | GAP_SCAN_READ_ADV_LIST_SIZE_EVENT 0x22 |
| Read period advertisers list size command complete event. More... | |
| #define | GAP_SCAN_REMOVE_DEVICE_ADV_LIST_EVENT 0x21 |
| Remove device from period advertisers list create sync command complete event. More... | |
| #define | GAP_SCAN_SESSION_END_EVENT 0x12 |
| Sent when an advertising report session ends. This is an internal event. More... | |
| #define | GAP_SCAN_SYNC_CANCEL_EVENT 0x1D |
| Periodic advertising create sync command complete event. More... | |
| #define | GAP_SCAN_TERMINATE_SYNC_EVENT 0x1E |
| Periodic advertising terminate sync command complete event. More... | |
| #define | GAP_SIGNATURE_UPDATED_EVENT 0x09 |
| #define | GAP_STATE_ADV 0x01U |
| Device is advertising. More... | |
| #define | GAP_STATE_IDLE 0x00U |
| Device is idle. More... | |
| #define | GAP_STATE_INIT 0x04U |
| Device is establishing a connection. More... | |
| #define | GAP_STATE_SCAN 0x02U |
| Device is scanning. More... | |
| #define | GAP_UPDATE_LINK_PARAM_REQ_EVENT 0x11 |
| #define | MASK_ADDRTYPE_ID 0x01 |
| AND with addrtype to remove ID from type. More... | |
| #define | PRIVATE_NON_RESOLVE_ADDR_HDR 0x80 |
| Random Private Non-Resolvable Address (b10) More... | |
| #define | PRIVATE_RESOLVE_ADDR_HDR 0x40 |
| Random Private Resolvable Address (b01) More... | |
| #define | RANDOM_ADDR_HDR_MASK 0xC0 |
| Get top 2 bits of address. More... | |
| #define | SET_ADDRTYPE_ID 0x02 |
| OR with addrtype to change addr type to ID. More... | |
| #define | STATIC_ADDR_HDR 0xC0 |
| Random Static Address (b11) More... | |
Typedefs | |
| typedef void(* | pfnGapCB_t) (uint32_t event, void *pBuf, uintptr_t arg) |
| typedef void(* | pfnGapConnEvtCB_t) (Gap_ConnEventRpt_t *pReport) |
| typedef uint8_t(* | pfnGapDevPrivModeCB_t) (GAP_Peer_Addr_Types_t addrType, uint8_t *pAddr) |
| GAP Device Privacy Mode Callback Function. More... | |
| typedef void(* | pfnGapIdleCB_t) () |
| GAP Idle Callback Function. More... | |
| typedef uint8_t(* | pfnSuppCentAddrRes_t) (uint8_t *deviceAddr, GAP_Peer_Addr_Types_t addrType) |
| Central Address Resolution (CAR) Support Callback Function. More... | |
Functions | |
| bStatus_t | GAP_Authenticate (gapAuthParams_t *pParams, gapPairingReq_t *pPairReq) |
| bStatus_t | GAP_Bond (uint16_t connectionHandle, uint8_t authenticated, uint8_t secureConnections, smSecurityInfo_t *pParams, uint8_t startEncryption) |
| bStatus_t | gap_checkLtk_GapBondMgr (uint16_t connectionHandle) |
| Checks the Long Term Key (LTK) for a given connection using the GAP Bond Manager. If GAP Bond Manager is used, this function will always return SUCCESS because the LTK is stored in the bond manager. More... | |
| bStatus_t | gap_checkLtk_noGapBondMgr (uint16_t connectionHandle) |
| Checks the Long Term Key (LTK) for a given connection without using the GAP Bond Manager. More... | |
| bStatus_t | GAP_DeviceInit (uint8_t profileRole, uint8_t taskID, GAP_Addr_Modes_t addrMode, uint8_t *pRandomAddr) |
| uint8_t * | GAP_GetDevAddress (uint8 wantIA) |
| uint8 * | GAP_GetDevAddressByType (uint8 wantIA, uint8 deviceAddrType) |
| uint8_t * | GAP_GetIRK (void) |
| uint16_t | GAP_GetParamValue (uint16_t paramID) |
| uint8_t * | GAP_GetSRK (void) |
| void | GAP_Init (uint8_t task_id) |
| uint8_t | GAP_isPairing (void) |
| uint8_t | GAP_NumActiveConnections (void) |
| bStatus_t | GAP_PasscodeUpdate (uint32_t passcode, uint16_t connectionHandle) |
| bStatus_t | GAP_PasskeyUpdate (uint8_t *pPasskey, uint16_t connectionHandle) |
| uint32 | GAP_ProcessEvent (uint8_t task_id, uint32 events) |
| void | GAP_RegisterBondMgrCBs (gapBondMgrCBs_t *pCBs) |
| bStatus_t | Gap_RegisterConnEventCb (pfnGapConnEvtCB_t cb, GAP_CB_Action_t action, GAP_CB_Event_e event, uint16_t connHandle) |
| void | GAP_RegisterForMsgs (uint8_t taskID) |
| bStatus_t | Gap_ReplyToLTKReq (uint16_t connectionHandle, smSecurityInfo_t *const pParams, uint8_t *isLTKUpdated) |
| bStatus_t | GAP_SendPeripheralSecurityRequest (uint16_t connectionHandle, uint8_t authReq) |
| bStatus_t | GAP_SetParamValue (uint16_t paramID, uint16_t paramValue) |
| bStatus_t | GAP_SetPrivacyMode (GAP_Peer_Addr_Types_t addrType, uint8_t *pAddr, uint8_t mode) |
| bStatus_t | GAP_Signable (uint16_t connectionHandle, uint8_t authenticated, smSigningInfo_t *pParams) |
| bStatus_t | GAP_TerminateAuth (uint16_t connectionHandle, uint8_t reason) |
| bStatus_t | GAP_TerminateLinkReq (uint16_t connectionHandle, uint8_t reason) |
| bStatus_t | GAP_UpdateLinkParamReq (gapUpdateLinkParamReq_t *pParams) |
| bStatus_t | GAP_UpdateLinkParamReqReply (gapUpdateLinkParamReqReply_t *pParams) |
| bStatus_t | GapConfig_SetParameter (Gap_configParamIds_t param, void *pValue) |