![]() |
![]() |
|
TI BLE5-Stack API Documentation
9.14.02
|
Go to the source code of this file.
Macros | |
| #define | STEP_HDR_LEN 3U |
| csSubeventResultsStep_t header length More... | |
Typedefs | |
| typedef void(* | pfnCsCB_t) (void *pEvt) |
| #define STEP_HDR_LEN 3U |
csSubeventResultsStep_t header length
| typedef void(* pfnCsCB_t) (void *pEvt) |
| enum csEventOpcodes_e |
| Enumerator | |
|---|---|
| CS_READ_REMOTE_SUPPORTED_CAPABILITIES_COMPLETE_EVENT | CS event Remote capabilities complete CS_readRemoteCapabEvt_t. |
| CS_READ_REMOTE_FAE_TABLE_COMPLETE_EVENT | CS event Read Remote FAE Table Complete CS_readRemFAECompleteEvt_t. |
| CS_SECURITY_ENABLE_COMPLETE_EVENT | CS Event Security Enable Complete CS_securityEnableCompleteEvt_t. |
| CS_CONFIG_COMPLETE_EVENT | CS event create config complete CS_configCompleteEvt_t. |
| CS_PROCEDURE_ENABLE_COMPLETE_EVENT | CS Procedure Enable Complete CS_procEnableCompleteEvt_t. |
| CS_SUBEVENT_RESULT | CS Subevent Result CS_subeventResultsEvt_t. |
| CS_SUBEVENT_CONTINUE_RESULT | CS Subevent continue Result CS_subeventResultsContinueEvt_t. |
| uint8_t CS_calcAntPathsMask | ( | csACI_e | aci | ) |
| uint8_t CS_calcNumPaths | ( | csACI_e | aci | ) |
| uint8_t CS_calcNumPathsFromAntennaMask | ( | uint8_t | antPathMask | ) |
| csStatus_e CS_CreateConfig | ( | CS_createConfigCmdParams_t * | params | ) |
| csStatus_e CS_GetRole | ( | CS_GetRoleCmdParams_t * | pParams | ) |
| uint8_t CS_GetStepLength | ( | uint8_t | mode, |
| uint8_t | role, | ||
| uint8_t | numAntennaPath | ||
| ) |
| csStatus_e CS_ProcedureEnable | ( | CS_setProcedureEnableCmdParams_t * | params | ) |
| void CS_ProcessEvent | ( | csEvtHdr_t * | pData | ) |
| csStatus_e CS_ReadLocalSupportedCapabilities | ( | csCapabilities_t * | localCapab | ) |
| csStatus_e CS_ReadRemoteFAETable | ( | CS_readRemoteFAETableCmdParams_t * | params | ) |
| csStatus_e CS_ReadRemoteSupportedCapabilities | ( | CS_readRemoteCapCmdParams_t * | params | ) |
| uint8_t CS_RegisterCB | ( | const csCBs_t * | pCBs | ) |
| csStatus_e CS_RemoveConfig | ( | CS_removeConfigCmdParams_t * | params | ) |
| csStatus_e CS_SecurityEnable | ( | CS_securityEnableCmdParams_t * | params | ) |
| csStatus_e CS_SetChannelClassification | ( | CS_setChannelClassificationCmdParams_t * | params | ) |
| csStatus_e CS_SetDefaultAntenna | ( | CS_setDefaultAntennaCmdParams_t * | pParams | ) |
| csStatus_e CS_SetDefaultSettings | ( | CS_setDefaultSettingsCmdParams_t * | params | ) |
| csStatus_e CS_SetProcedureParameters | ( | CS_setProcedureParamsCmdParams_t * | params | ) |
| csStatus_e CS_WriteCachedRemoteFAETable | ( | CS_writeCachedRemoteFAETableCmdParams_t * | params | ) |
| csStatus_e CS_WriteCachedRemoteSupportedCapabilities | ( | CS_writeCachedRemoteCapCmdParams_t * | pParams | ) |