CC23xx or CC27xx SDK 8.40 to CC23xx or CC27xx SDK 9.10

This section will describe how to port a project from CC23xx or CC27xx SDK 8.40 to a CC23xx or CC27xx SDK 9.10 project.

Note

Vulnerability reports and mitigations can be found on Report potential product security vulnerabilities.

Porting Bluetooth LE Projects

The recommended method for porting an existing project from CC23xx or CC27xx SDK 8.40 to CC23xx or CC27xx SDK 9.10 is to modify the project using only the Code Composer Studio interface. The following steps will detail the changes needed when porting an out of the box example from the SDK such as basic_ble:

  1. Import the project into Code Composer Studio.

2. In order to modify the SDK version, corresponding SysConfig version, as well as the compiler version, right-click on the imported project folder inside the Project Explorer and select Properties.

3. In General, select Compiler and choose the correct version. Refer to the Dependencies section in the SDK release notes

../../../_images/8.40_to_9.10_compiler.png

Figure 249. Code Composer Studio - Change Compiler Version.

4. Go to Dependencies and double-click on SimpleLink Low Power F3 SDK and choose the correct version. Then double-click on SysConfig and do the same. Refer to the Dependencies Section in the SDK release notes for the correct versions.

../../../_images/8.40_to_9.10_sdk.png

Figure 250. Code Composer Studio - Change SDK and SysConfig Version.

If the newest SDK is not available, it will need to be actualized. To do this, go to File => Preferences => Code Composer Studio Settings, and select Products. Inside the Products tab, press the refresh button, which should discover the latest version of the SDK that was installed.

  1. Go to Arm Compiler and select Include Options. In there, remove the following include paths:

    1. All paths that include ble5stack_flash

    2. ${COM_TI_SIMPLELINK_LOWPOWER_F3_SDK_INSTALL_DIR}/source/ti/bleapp/profiles/health_thermometer

    3. ${COM_TI_SIMPLELINK_LOWPOWER_F3_SDK_INSTALL_DIR}/source/ti/bleapp/services/health_thermometer

  2. Go to Advanced Options and select Command files. In there, remove the two file paths and add:

    1. ${COM_TI_SIMPLELINK_LOWPOWER_F3_SDK_INSTALL_DIR}/source/ti/ble/stack_util/config/build_components.opt

    2. ${COM_TI_SIMPLELINK_LOWPOWER_F3_SDK_INSTALL_DIR}/source/ti/ble/stack_util/config/factory_config.opt

7. Exit the Properties menu. Right-click the SysConfig file in the project and select “Open With”, then select “Text Editor”. Then, inside the SysConfig file, change all instances of ble5stack to ble.

8. Due to a change in the naming conventions, the following changes are needed for each instance of the following paths:

Table 37. File Renaming

Change from

Change to

source/ti/ble5stack_flash

source/ti/ble

source/ti/ble5stack_flash/lib_projects

source/ti/ble/lib

source/ti/bleapp/services

source/ti/ble/services

source/ti/bleapp/profiles

source/ti/ble/profiles

source/ti/bleapp

source/ti/ble/app_util

tools/ble5stack

tools/ble

source/ti/ble/app_util/util/sw_update

source/ti/ble/app_util/sw_update

source/ti/bleapp/ble_app_util

source/ti/ble/app_util/framework

source/ti/bleapp/ble_app_util/inc

source/ti/ble/app_util/framework

source/ti/bleapp/menu_module

source/ti/ble/app_util/menu

source/ti/ble5stack/.meta

source/ti/ble/.meta

source/ti/ble5stack_flash

source/t/ble/host

source/ti/ble5stack_flash/npi

source/ti/ble/app_util/npi

source/ti/ble5stack_flash/npi/unified

source/ti/ble/app_util/unpi

source/ti/ble5stack_flash/health_toolkit

source/ti/ble/stack_util

source/ti/ble5stack_flash/osal

source/ti/ble/stack_util/osal

source/ti/ble5stack_flash/icall

source/ti/ble/stack_util/icall

source/ti/ble5stack_flash/rom

source/ti/ble/stack_util/lib_opt

source/ti/ble5stack_flash/config

source/ti/ble/stack_util/config

  1. Go to common => Startup and click on ocal_icall_ble.c and edit the following:

    1. Since the previous include paths were taken out in the properties section of the project, the following include paths will need to be changed:

    Table 38. Include path changes in osal_icall_ble.c

    Change from

    Change to

    #include “osal_snv.h”

    #include “ti/ble/stack_util/osal/osal_snv.h”

    #include “osal.h”

    #include “ti/ble/stack_util/osal/osal.h”

    #include <icall.h>

    #include “ti/ble/stack_util/icall/app/icall.h”

    #include “hal_types.h” and #include “hal_mcu.h”

    #include “ti/ble/stack_util/comdef.h”

    #include “osal_tasks.h”

    #include “ti/ble/stack_util/osal/osal_tasks.h”

    #include “ll.h”

    #include “ti/ble/controller/ll/ll.h”

    #include “osal_cbtimer.h”

    #include “ti/ble/stack_util/osal/osal_cbtimer.h”

    #include “l2cap.h”

    #include “ti/ble/host/l2cap/l2cap.h”

    #include “gap.h”

    #include “ti/ble/host/gap/gap.h”

    #include “gapbondmgr_internal.h”

    #include “ti/ble/host/gapbondmgr/gapbondmgr_internal.h”

    #include “gatt.h”

    #include “ti/ble/host/gatt/gatt.h”

    #include “hci_tl.h”

    #include “ti/ble/controller/hci/hci_tl.h”

    #include “gattservapp.h”

    #include “ti/ble/host/gatt/gattservapp.h”

    #include “gapbondmgr.h”

    #include “ti/ble/host/gapbondmgr/gapbondmgr.h”

    #include “ble_user_config.h”

    #include “ti/ble/app_util/config/ble_user_config.h”

    #include “ble_dispatch.h”

    #include “ti/ble/stack_util/icall/stack/ble_dispatch_lite.h”

    1. Inside tasksArr:

      #ifdef ICALL_LITE
        ble_dispatch_liteProcess,                                         // task 9
      #else
        bleDispatch_ProcessEvent                                          // task 9
      #endif /* ICALL_LITE */
      

    Would become:

    ble_dispatch_liteProcess
    
    1. Inside osalInitTasks:

      #ifdef ICALL_LITE
        ble_dispatch_liteInit(taskID++);
      #else
        /* ICall BLE Dispatcher Task */
        bleDispatch_Init( taskID );
      
      #endif /* ICALL_LITE */
      

      Would become:

      ble_dispatch_liteInit(taskID++);
      
    2. Inside osalInitTasks, remove:

      #ifndef ICALL_LITE
        /* Enroll the obtained dispatcher entity and OSAL task ID of HCI Ext App
        * to OSAL so that OSAL can route the dispatcher message into
        * the appropriate OSAL task.
        */
        osal_enroll_dispatchid(taskID, entity);
      #endif /* ICALL_LITE */
      
    3. Inside stack_main:

      #ifdef ICALL_JT
        setBleUserConfig( (icall_userCfg_t *)arg );
      #else /* !(ICALL_JT) */
        setBleUserConfig( (bleUserCfg_t *)arg );
      #endif /* ICALL_JT *
      

      Would become:

      setBleUserConfig( (icall_userCfg_t *)arg );
      
    4. Inside stack_main:

      #if defined(ICALL_LITE) && (!defined(STACK_LIBRARY))
        {
          icall_liteTranslationInit((uint32_t*)bleAPItable);
        }
      #endif  /* ICALL_LITE */
      
      #ifdef ICALL_LITE
        {
          osal_set_icall_hook(icall_liteMsgParser);
        }
      #endif  /* ICALL_LITE */
      

      Would become:

      osal_set_icall_hook(icall_liteMsgParser);
      
    5. Inside stack_main, remove the following lines:

      #ifdef CC23X0
      #ifndef USE_HSM
        if (LL_initRNGNoise() != LL_STATUS_SUCCESS)
        {
        /* abort */
          ICall_abort();
        }
      #endif
      #endif
      
  2. Go to main_freertos.c and edit the following:

  1. Remove the following includes: #include <ti/common/cc26xx/uartlog/UartLog.h> and #include “ble_stack_api.h”

  2. Change the following includes:

    Table 39. Include path changes in main_freertos.c

    Change from

    Change to

    #include <icall.h>

    #include “ti/ble/stack_util/icall/app/icall.h”

    #include “hal_assert.h”

    #include “ti/ble/stack_util/health_toolkit/assert.h”

    #include “bcomdef.h”

    #include “ti/ble/stack_util/bcomdef.h”

    #include “ble_user_config.h”

    #include “ti/ble/app_util/config/ble_user_config.h”

  3. Turn all log_error0 instances into HAL_ASSERT_SPINLOCK, and remove the log_error2 instance.

  1. Delete the following files from the project:

  1. ble_stack_api.c inside of iCallBLE folder

  2. ble_stack_api.h inside of iCallBLE folder

  3. icall_api_lite.c inside of iCallBLE folder

  4. ble_user_config_stack.c inside of Startup folder

  1. Import basic_ble from the CC23xx or CC27xx SDK 9.10 SDK, copy the “lib_opt” folder and paste it in the example you are attempting to migrate.

  2. Some files inside the project will still be unresolved, due to the location change. To fix this:

  1. Copy the path of the file. Each file’s correct path is included in the table below

  2. Right-click on the unresolved file

  3. Select “Edit Linked File”

  4. Replace the current path with the one copied from the table below

Table 40. Linked File Paths

File

Path

bleapputil_api.h

${COM_TI_SIMPLELINK_LOWPOWER_F3_SDK_INSTALL_DIR}/source/ti/ble/app_util/framework/bleapputil_api.h

bleaputil_init.c

${COM_TI_SIMPLELINK_LOWPOWER_F3_SDK_INSTALL_DIR}/source/ti/ble/app_util/framework/src/bleapputil_init.c

bleapputil_process.c

${COM_TI_SIMPLELINK_LOWPOWER_F3_SDK_INSTALL_DIR}/source/ti/ble/app_util/framework/src/bleapputil_process.c

bleapputil_stack_callbacks.c

${COM_TI_SIMPLELINK_LOWPOWER_F3_SDK_INSTALL_DIR}/source/ti/ble/app_util/framework/src/bleapputil_stack_callbacks.c

bleapputil_task.c

${COM_TI_SIMPLELINK_LOWPOWER_F3_SDK_INSTALL_DIR}/source/ti/ble/app_util/framework/src/bleapputil_task.c

icall_addrs.h

${COM_TI_SIMPLELINK_LOWPOWER_F3_SDK_INSTALL_DIR}/source/ti/ble/stack_util/icall/app/icall_addrs.h

icall_cc23x0.c

${COM_TI_SIMPLELINK_LOWPOWER_F3_SDK_INSTALL_DIR}/source/ti/ble/stack_util/icall/app/src/icall_cc23x0.c

icall_platform.h

${COM_TI_SIMPLELINK_LOWPOWER_F3_SDK_INSTALL_DIR}/source/ti/ble/stack_util/icall/app/icall_platform.h

icall_POSIX.c

${COM_TI_SIMPLELINK_LOWPOWER_F3_SDK_INSTALL_DIR}/source/ti/ble/stack_util/icall/app/src/icall_POSIX.c

icall_user_config.c

${COM_TI_SIMPLELINK_LOWPOWER_F3_SDK_INSTALL_DIR}/source/ti/ble/stack_util/icall/app/src/icall_user_config.c

icall_user_config.h

${COM_TI_SIMPLELINK_LOWPOWER_F3_SDK_INSTALL_DIR}/source/ti/ble/stack_util/icall/app/icall_user_config.h

icall.h

${COM_TI_SIMPLELINK_LOWPOWER_F3_SDK_INSTALL_DIR}/source/ti/ble/stack_util/icall/app/icall.h

ble_user_config.c

${COM_TI_SIMPLELINK_LOWPOWER_F3_SDK_INSTALL_DIR}/source/ti/ble/app_util/config/src/ble_user_config.c

ble_user_config.h

${COM_TI_SIMPLELINK_LOWPOWER_F3_SDK_INSTALL_DIR}/source/ti/ble/app_util/config/ble_user_config.h

icall_ble_apimsg.h

${COM_TI_SIMPLELINK_LOWPOWER_F3_SDK_INSTALL_DIR}/source/ti/ble/stack_util/icall/app/icall_ble_apimsg.h

menu_module.c

${COM_TI_SIMPLELINK_LOWPOWER_F3_SDK_INSTALL_DIR}/source/ti/ble/app_util/menu/src/menu_module.c

menu_module.h

${COM_TI_SIMPLELINK_LOWPOWER_F3_SDK_INSTALL_DIR}/source/ti/ble/app_util/menu/menu_module.h

simple_gatt_profile.c

${COM_TI_SIMPLELINK_LOWPOWER_F3_SDK_INSTALL_DIR}/source/ti/ble/app_util/menu/src/menu_module.c

simple_gatt_profile.h

${COM_TI_SIMPLELINK_LOWPOWER_F3_SDK_INSTALL_DIR}/source/ti/ble/profiles/simple_gatt/simple_gatt_profile.h

dev_info_service.c

${COM_TI_SIMPLELINK_LOWPOWER_F3_SDK_INSTALL_DIR}/source/ti/ble/services/dev_info/src/dev_info_service.c

dev_info_service.h

${COM_TI_SIMPLELINK_LOWPOWER_F3_SDK_INSTALL_DIR}/source/ti/ble/services/dev_info/dev_info_service.h

rom_init.c

${COM_TI_SIMPLELINK_LOWPOWER_F3_SDK_INSTALL_DIR}/source/ti/ble/stack_util/lib_opt/rom_init.c

Note

These edits pertain to the basic_ble project. Other projects may require similar edits to other files as well!

Legacy Porting

Warning

The following section covers a legacy porting method. Current SDK porting does not require this process and should instead see Porting Bluetooth LE Projects.

For this guide, a peripheral project from CC23xx or CC27xx SDK 8.40 will be ported over to CC23xx or CC27xx SDK 9.10. The recommended approach is to start with the Basic BLE project on CC23xx or CC27xx SDK 9.10 and modify the base configuration to match the peripheral configuration used in the CC23xx or CC27xx SDK 8.40 project. Afterwards, the custom application code should be transferred to the new project.

  1. Import a CC23xx or CC27xx SDK 9.10 Basic BLE project.

  2. Change the default Basic BLE project configuration options in the BLE Module present in SysConfig to match the configuration used in the CC23xx or CC27xx SDK 8.40 project.

  3. Transfer all custom application logic from the CC23xx or CC27xx SDK 8.40 into the CC23xx or CC27xx SDK 9.10 Basic BLE project.

  4. Move any profiles and services that the application is using to the CC23xx or CC27xx SDK 9.10 project.

  5. Transfer the SysConfig settings either visually through the GUI or open both the old and the new project .syscfg files and copy-paste the desired settings.

  6. If necessary, update the project to use the newer TI drivers that are supplied with the SimpleLink Low Power F3 SDK. Additional details are provided in A Few Noteworthy Changes from CC23xx or CC27xx SDK 8.40 to CC23xx or CC27xx SDK 9.10.

  7. Refer to the Core SDK release notes for additional information and the FreeRTOS examples included with SimpleLink Low Power F3 SDK. The Core SDK release notes may be found in {SDK_INSTALL_DIR}/docs/simplelink_mcu_sdk/release_notes_coresdk_lpf3_x_xx_xx_xx.html

    For additional information on how CC23xx or CC27xx SDK 9.10 uses FreeRTOS see FreeRTOS (RTOS Kernel) Overview.

    For any utilized TI Drivers, review TI Drivers API Reference.

A Few Noteworthy Changes from CC23xx or CC27xx SDK 8.40 to CC23xx or CC27xx SDK 9.10

You can follow the guide above without addressing these updates; they are listed for your information only. All fine grained details might not be mentioned. However, please keep in mind that the file name changes need to be addressed regardless of the project being migrated.

Also, due to the crypto drivers being removed from the drivers library and moved into a seperate secure drivers library, the lib folder will need to be added (source/ti/drivers/secure/lib). Please refer to the specific example you need to port and do a compare between the old and new project files.

Please refer to the BLE5-Stack Release Notes for all the details.