|
API Documentation
9.14.01
|
Macros | |
| #define | UART2_STATUS_EAGAIN (-16) |
| A UART2_write() or UART2_read() in UART2_Mode_NONBLOCKING would have blocked. | |
| #define | UART2_STATUS_EBREAK (-4) |
| A break error occurred. | |
| #define | UART2_STATUS_ECANCELLED (-14) |
| A UART2_write() or UART2_read() operation was cancelled. | |
| #define | UART2_STATUS_EFAIL (-11) |
| General failure status returned by UART2 API. | |
| #define | UART2_STATUS_EFRAMING (-1) |
| A framing error occurred. | |
| #define | UART2_STATUS_EINUSE (-9) |
| The UART is currently in use. | |
| #define | UART2_STATUS_EINVALID (-10) |
| An invalid argument or UART2_Params field was passed to UART2 API. | |
| #define | UART2_STATUS_EMEMORY (-12) |
| A memory allocation failure occurred. | |
| #define | UART2_STATUS_ENOTOPEN (-15) |
| A UART2_write() or UART2_read() called on a device not opened. | |
| #define | UART2_STATUS_EOVERRUN (-8) |
| A FIFO overrun occurred. | |
| #define | UART2_STATUS_EPARITY (-2) |
| A parity error occurred. | |
| #define | UART2_STATUS_ETIMEOUT (-13) |
| A timeout occurred for a blocking UART2_read or UART2_write call. | |
| #define | UART2_STATUS_SREADTIMEOUT (1) |
| A read timeout occurred (not an error). | |
| #define | UART2_STATUS_SUCCESS (0) |
| Successful status code returned by UART2 APIs. | |
1.8.12