API Documentation  9.14.01
Data Structures
Here are the data structures with brief descriptions:
 CADC_Config_ADC driver's custom configuration structure
 CADC_FxnTableThe definition of an ADC function table that contains the required set of functions to control a specific ADC driver implementation
 CADC_ParamsADC Parameters used with ADC_open()
 CADCBuf_Config_ADC driver's custom configuration structure
 CADCBuf_ConversionDefines a conversion to be used with ADCBuf_convert()
 CADCBuf_FxnTableThe definition of an ADCBuf function table that contains the required set of functions to control a specific ADC driver implementation
 CADCBuf_ParamsADCBuf parameters used with ADCBuf_open()
 CADCBufCC26XX_AdcChannelLutEntryTable entry that maps a virtual adc channel to a dio and its corresponding internal analogue signal
 CADCBufCC26XX_HWAttrsADCBufCC26XX Hardware Attributes
 CADCBufCC26XX_ObjectADCBufCC26XX Object
 CADCBufCC26XX_ParamsExtensionCC26XX specfic extension to ADCBuf_Params
 CADCCC26XX_HWAttrsADCCC26XX Hardware attributes These fields are used by driverlib APIs and therefore must be populated by driverlib macro definitions
 CADCCC26XX_ObjectADCCC26XX Object
 CDisplay_ConfigDisplay Global configuration
 CDisplay_FxnTableThe definition of a Display function table that contains the required set of functions to control a specific Display driver implementation
 CDisplay_ParamsDisplay Parameters
 CDisplayDogm1286_HWAttrs
 CDisplayDogm1286_Object
 CDisplayGrLib_Object
 CDisplayHost_HWAttrsDisplayHost Attributes
 CDisplayHost_ObjectDisplayHost Object
 CDisplaySharp_HWAttrsV1
 CDisplaySharp_Object
 CDisplaySharpColor_tForeground and background color struct, compatible with GrLib
 CDisplayUart2_HWAttrsDisplayUart2 Attributes
 CDisplayUart2_ObjectDisplayUart2 Object
 CGPIO_ConfigGPIO driver configuration structure
 CGPTimerCC26XX_ConfigGPTimer Global configuration
 CGPTimerCC26XX_HWAttrsGPTimer26XX Hardware attributes
 CGPTimerCC26XX_ObjectGPTimer26XX Object
 CGPTimerCC26XX_ParamsGPTimerCC26XX Parameters
 CI2C_Config_I2C driver's custom configuration structure
 CI2C_ParamsI2C parameters used with I2C_open()
 CI2C_TransactionDefines a transaction to be used with I2C_transfer() or I2C_transferTimeout()
 CI2CCC26XX_HWAttrsV1I2CCC26XX Hardware attributes
 CI2CCC26XX_I2CPinCfgI2CCC26XX Pin Configuration
 CI2CCC26XX_ObjectI2CCC26XX Object
 CPDMCC26XX_BufferRequestA PDMCC26XX_BufferRequest data structure is used with PDMCC26XX_requestBuffer()
 CPDMCC26XX_ConfigThe PDMCC26XX_Config structure contains a set of pointers used to characterize the PDMCC26XX driver implementation
 CPDMCC26XX_HWAttrsPDMCC26XX Hardware attributes
 CPDMCC26XX_I2S_AudioClockConfigPDMCC26XX_I2S Audio Clock configuration
 CPDMCC26XX_I2S_AudioFormatConfigPDMCC26XX_I2S Hardware configuration
 CPDMCC26XX_I2S_AudioPinConfigPDMCC26XX_I2S Audio Pin configuration
 CPDMCC26XX_I2S_BufferReleaseA PDMCC26XX_I2S_BufferRelease data structure is used with PDMCC26XX_I2S_releaseBuffer()
 CPDMCC26XX_I2S_BufferRequestA PDMCC26XX_I2S_BufferRequest data structure is used with PDMCC26XX_I2S_requestBuffer()
 CPDMCC26XX_I2S_ConfigThe PDMCC26XX_I2S_Config structure contains a set of pointers used to characterize the PDMCC26XX_I2S driver implementation
 CPDMCC26XX_I2S_HWAttrsPDMCC26XX_I2S Hardware attributes
 CPDMCC26XX_I2S_ObjectPDMCC26XX_I2S Object
 CPDMCC26XX_I2S_ParamsPDMCC26XX I2S Parameters are used when calling PDMCC26XX_I2S_open()
 CPDMCC26XX_I2S_StreamNotificationA PDMCC26XX_I2S_StreamNotification data structure is used with PDMCC26XX_I2S_CallbackFxn(). Provides notification about available buffers and potential errors
 CPDMCC26XX_metaDataMetadata associated with an array of PCM data
 CPDMCC26XX_ObjectPDMCC26XX Object
 CPDMCC26XX_ParamsPDMCC26XX Parameters are used to with the PDMCC26XX_open() call. Default values for these parameters are set using PDMCC26XX_Params_init()
 CPDMCC26XX_pcmBufferPCM buffer pointed to in a PDMCC26XX_BufferRequest
 CPDMCC26XX_StreamNotificationA PDMCC26XX_StreamNotification data structure is used with PDMCC26XX_CallbackFxn(). Provides notification about available buffers and potential errors
 CPower_NotifyObjPower notify object structure
 CPowerCC26XX_ConfigGlobal configuration structure
 CPowerCC26XX_ModuleStatePowerCC26XX_ModuleState
 CPWM_Config_PWM Global configuration
 CPWM_FxnTableThe definition of a PWM function table that contains the required set of functions to control a specific PWM driver implementation
 CPWM_ParamsPWM Parameters
 CPWMTimerCC26XX_HwAttrsPWMTimer26XX Hardware attributes
 CPWMTimerCC26XX_ObjectPWMTimer26XX Object
 CSPI_Config_SPI Global configuration
 CSPI_FxnTableThe definition of a SPI function table that contains the required set of functions to control a specific SPI driver implementation
 CSPI_ParamsSPI Parameters
 CSPI_TransactionA SPI_Transaction data structure is used with SPI_transfer(). It indicates how many SPI_FrameFormat frames are sent and received from the buffers pointed to txBuf and rxBuf. The arg variable is an user-definable argument which gets passed to the SPI_CallbackFxn when the SPI driver is in SPI_MODE_CALLBACK
 CUART2_Config_UART2 Global configuration
 CUART2_ParamsUART2 Parameters
 CUDMACC26XX_ConfigUDMACC26XX Global configuration
 CUDMACC26XX_HWAttrsUDMACC26XX hardware attributes
 CUDMACC26XX_ObjectUDMACC26XX object
 CWatchdog_Config_Watchdog Global configuration
 CWatchdog_FxnTableThe definition of a Watchdog function table that contains the required set of functions to control a specific Watchdog driver implementation
 CWatchdog_ParamsWatchdog Parameters
 CWatchdogCC26XX_HWAttrsWatchdog hardware attributes for CC26XX
 CWatchdogCC26XX_ObjectWatchdog Object for CC26XX