|
API Documentation
9.14.01
|
Display.h implementation for UART output. More...
Go to the source code of this file.
Data Structures | |
| struct | DisplayUart2_HWAttrs |
| DisplayUart2 Attributes. More... | |
| struct | DisplayUart2_Object |
| DisplayUart2 Object. More... | |
Macros | |
| #define | DisplayUart2_SCROLLING 0xFF |
Typedefs | |
| typedef struct DisplayUart2_Object * | DisplayUart2_Handle |
Functions | |
| void | DisplayUart2Ansi_clear (Display_Handle handle) |
| void | DisplayUart2Ansi_clearLines (Display_Handle handle, uint8_t fromLine, uint8_t toLine) |
| void | DisplayUart2Ansi_close (Display_Handle handle) |
| int | DisplayUart2Ansi_control (Display_Handle handle, unsigned int cmd, void *arg) |
| unsigned int | DisplayUart2Ansi_getType (void) |
| void | DisplayUart2Ansi_init (Display_Handle handle) |
| Display_Handle | DisplayUart2Ansi_open (Display_Handle handle, Display_Params *params) |
| void | DisplayUart2Ansi_vprintf (Display_Handle handle, uint8_t line, uint8_t column, const char *fmt, va_list va) |
| void | DisplayUart2Min_clear (Display_Handle handle) |
| void | DisplayUart2Min_clearLines (Display_Handle handle, uint8_t fromLine, uint8_t toLine) |
| void | DisplayUart2Min_close (Display_Handle handle) |
| int | DisplayUart2Min_control (Display_Handle handle, unsigned int cmd, void *arg) |
| unsigned int | DisplayUart2Min_getType (void) |
| void | DisplayUart2Min_init (Display_Handle handle) |
| Display_Handle | DisplayUart2Min_open (Display_Handle handle, Display_Params *params) |
| void | DisplayUart2Min_vprintf (Display_Handle handle, uint8_t line, uint8_t column, const char *fmt, va_list va) |
Variables | |
| const Display_FxnTable | DisplayUart2Ansi_fxnTable |
| const Display_FxnTable | DisplayUart2Min_fxnTable |
Display.h implementation for UART output.
============================================================================
DisplayUart2 has two sets of function pointer tables. One which adds some ANSI/VT100 codes to the output, for cursor placement etc, and a minimal implementation which basically is a wrapper for UART2_write.
DisplayUart2Min simply formats and outputs the text over UART and adds a newline at the end of each statement.
Calls to Display_clear, Display_clearLine(s), and the line and column specifiers in Display_printf(handle, line, col, fmt, ...) are ignored.
DisplayUart2Ansi will send the following escape-strings to the UART when it is opened:
When Display_print(handle, line, col, fmt, ...) is called with a line number the following is sent:
If Display_printf is called with the line "number" DisplayUart2_SCROLLING, the string to be printed is simply output at the current cursor location, without saving or restoring the position. If the terminal supports the scrolling region feature, as most do, then the terminal will ensure that the content output here will scroll up but not overwrite the text written outside the scroll region.
In this manner it is possible to have two separate outputs, one with a log of events, and one with fixed positions as on an LCD. Unless the DisplayUart_SCROLLING line specifier is used, any line number can be used, also those nominally inside the scrolling region.
There is also a helper file <ti/display/AnsiColor.h> with a macro to set the color and style of the text.
1.8.12