TI OAD API Documentation  9.14.01
Functions
Random generation

Functions

psa_status_t psa_generate_key (const psa_key_attributes_t *attributes, psa_key_id_t *key)
 Generate a key or key pair. More...
 
psa_status_t psa_generate_random (uint8_t *output, size_t output_size)
 Generate random bytes. More...
 

Detailed Description

Function Documentation

§ psa_generate_key()

psa_status_t psa_generate_key ( const psa_key_attributes_t *  attributes,
psa_key_id_t *  key 
)

Generate a key or key pair.

The key is generated randomly. Its location, usage policy, type and size are taken from attributes.

Implementations must reject an attempt to generate a key of size 0.

The following type-specific considerations apply:

  • For RSA keys (#PSA_KEY_TYPE_RSA_KEY_PAIR), the public exponent is 65537. The modulus is a product of two probabilistic primes between 2^{n-1} and 2^n where n is the bit size specified in the attributes.
Parameters
[in]attributesThe attributes for the new key.
[out]keyOn success, an identifier for the newly created key. For persistent keys, this is the key identifier defined in attributes. 0 on failure.
Return values
#PSA_SUCCESSSuccess. If the key is persistent, the key material and the key's metadata have been saved to persistent storage.
#PSA_ERROR_ALREADY_EXISTSThis is an attempt to create a persistent key, and there is already a persistent key with the given identifier.
#PSA_ERROR_NOT_SUPPORTED
#PSA_ERROR_INVALID_ARGUMENT
#PSA_ERROR_INSUFFICIENT_MEMORY
#PSA_ERROR_INSUFFICIENT_ENTROPY
#PSA_ERROR_COMMUNICATION_FAILURE
#PSA_ERROR_HARDWARE_FAILURE
#PSA_ERROR_CORRUPTION_DETECTED
#PSA_ERROR_INSUFFICIENT_STORAGE
#PSA_ERROR_DATA_INVALID
#PSA_ERROR_DATA_CORRUPT
#PSA_ERROR_STORAGE_FAILURE
#PSA_ERROR_BAD_STATEThe library has not been previously initialized by psa_crypto_init(). It is implementation-dependent whether a failure to initialize results in this error code.

§ psa_generate_random()

psa_status_t psa_generate_random ( uint8_t *  output,
size_t  output_size 
)

Generate random bytes.

Warning
This function can fail! Callers MUST check the return status and MUST NOT use the content of the output buffer if the return status is not #PSA_SUCCESS.
Note
To generate a key, use psa_generate_key() instead.
Parameters
[out]outputOutput buffer for the generated data.
output_sizeNumber of bytes to generate and output.
Return values
#PSA_SUCCESS
#PSA_ERROR_NOT_SUPPORTED
#PSA_ERROR_INSUFFICIENT_ENTROPY
#PSA_ERROR_INSUFFICIENT_MEMORY
#PSA_ERROR_COMMUNICATION_FAILURE
#PSA_ERROR_HARDWARE_FAILURE
#PSA_ERROR_CORRUPTION_DETECTED
#PSA_ERROR_BAD_STATEThe library has not been previously initialized by psa_crypto_init(). It is implementation-dependent whether a failure to initialize results in this error code.