TI BLE5-Stack API Documentation  9.14.01
Data Fields
l2capPsmInfo_t Struct Reference

PSM information format. More...

Data Fields

uint16 initPeerCredits
 Number of LE-frames that peer device can send. More...
 
uint8 maxNumChannels
 Maximum number of CO Channels supported by PSM. More...
 
uint16 mps
 Maximum payload size that can be received by local device. More...
 
uint16 mtu
 Maximum SDU size that can be received by local device. More...
 
uint8 numActiveChannels
 Number of active CO Channels. More...
 
uint16 peerCreditThreshold
 Low threshold for number of peer credits. More...
 

Detailed Description

PSM information format.

Field Documentation

§ initPeerCredits

uint16 initPeerCredits

Number of LE-frames that peer device can send.

§ maxNumChannels

uint8 maxNumChannels

Maximum number of CO Channels supported by PSM.

§ mps

uint16 mps

Maximum payload size that can be received by local device.

§ mtu

uint16 mtu

Maximum SDU size that can be received by local device.

§ numActiveChannels

uint8 numActiveChannels

Number of active CO Channels.

§ peerCreditThreshold

uint16 peerCreditThreshold

Low threshold for number of peer credits.


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale