![]() |
![]() |
|
TI BLE5-Stack API Documentation
9.14.01
|
Number of Completed Packets Event. More...
Data Fields | |
| event_hdr_t | hdr |
| osal event header More... | |
| uint8 | numHandles |
| number of handles More... | |
| uint16 * | pConnectionHandle |
| pointer to the connection handle array More... | |
| uint16 * | pNumCompletedPackets |
| pointer to the number of completed packets array More... | |
Number of Completed Packets Event.
| event_hdr_t hdr |
osal event header
| uint8 numHandles |
number of handles
| uint16* pConnectionHandle |
pointer to the connection handle array
| uint16* pNumCompletedPackets |
pointer to the number of completed packets array