![]() |
![]() |
|
TI BLE5-Stack API Documentation
9.14.01
|
Command Complete Event. More...
Data Fields | |
| uint16 | cmdOpcode |
| command opcode More... | |
| event_hdr_t | hdr |
| osal event header More... | |
| uint8 | numHciCmdPkt |
| number of HCI Command Packet More... | |
| uint8 * | pReturnParam |
| pointer to the return parameter More... | |
Command Complete Event.
| uint16 cmdOpcode |
command opcode
| event_hdr_t hdr |
osal event header
| uint8 numHciCmdPkt |
number of HCI Command Packet
| uint8* pReturnParam |
pointer to the return parameter