![]() |
![]() |
|
TI BLE5-Stack API Documentation
9.14.01
|
Data Fields | |
| uint8 | BLEEventCode |
| BLE Event Code. More... | |
| uint16 | connHandle |
| Connection handle. More... | |
| uint8 | delta |
| The change of the Tx Power from previous power level. More... | |
| event_hdr_t | hdr |
| Osal event header. More... | |
| uint8 | reason |
| Who trigger the event - local or remote. More... | |
| uint8 | status |
| status of event More... | |
| uint8 | txPhy |
| On which phy the report is trigger. More... | |
| uint8 | txPowerFlag |
| Tx Power at minimum or maximum level. More... | |
| uint8 | txPowerLevel |
| Amount of power transmitting. More... | |
| uint8 BLEEventCode |
BLE Event Code.
| uint16 connHandle |
Connection handle.
| uint8 delta |
The change of the Tx Power from previous power level.
| event_hdr_t hdr |
Osal event header.
| uint8 reason |
Who trigger the event - local or remote.
| uint8 status |
status of event
| uint8 txPhy |
On which phy the report is trigger.
| uint8 txPowerFlag |
Tx Power at minimum or maximum level.
| uint8 txPowerLevel |
Amount of power transmitting.