TI BLE5-Stack API Documentation  9.14.01
Data Fields
hciEvt_BLEReadRemoteFeatureComplete_t Struct Reference

LE Read Remote Used Features Complete Event. More...

Data Fields

uint8 BLEEventCode
 BLE Event Code. More...
 
uint16 connectionHandle
 connection handle More...
 
uint8 features [8]
 features More...
 
event_hdr_t hdr
 osal event header More...
 
uint8 status
 status of event More...
 

Detailed Description

LE Read Remote Used Features Complete Event.

Field Documentation

§ BLEEventCode

uint8 BLEEventCode

BLE Event Code.

§ connectionHandle

uint16 connectionHandle

connection handle

§ features

uint8 features[8]

features

§ hdr

osal event header

§ status

uint8 status

status of event


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale