TI BLE5-Stack API Documentation  9.14.01
Data Fields
hciEvt_BLEExtCteConnectionIqReport_t Struct Reference

LE Extended CTE Connection IQ Report Event. More...

Data Fields

uint8 BLEEventCode
 BLE Event Code. More...
 
uint16 connEvent
 connection event More...
 
uint16 connHandle
 connection handle More...
 
uint8 cteType
 cte type More...
 
uint8 dataChIndex
 index of data channel More...
 
uint8 dataLen
 samples data length More...
 
uint8 eventIndex
 event number More...
 
event_hdr_t hdr
 osal event header More...
 
void * iqSamples
 list of interleaved I/Q samples (list size is dataLen*2) More...
 
uint8 phy
 current phy More...
 
uint16 rssi
 current rssi More...
 
uint8 rssiAntenna
 antenna ID More...
 
uint8 sampleCtrl
 sample control - default filtering or RAW_RF More...
 
uint8 sampleRate
 sample rate (1/2/3/4 MHz) More...
 
uint8 sampleSize
 sample size (8 or 16 bit) More...
 
uint8 slotDuration
 sampling slot 1us or 2us More...
 
uint8 status
 packet status (success or CRC error) More...
 
uint16 totalDataLen
 samples data length includes in all next events More...
 

Detailed Description

LE Extended CTE Connection IQ Report Event.

Field Documentation

§ BLEEventCode

uint8 BLEEventCode

BLE Event Code.

§ connEvent

uint16 connEvent

connection event

§ connHandle

uint16 connHandle

connection handle

§ cteType

uint8 cteType

cte type

§ dataChIndex

uint8 dataChIndex

index of data channel

§ dataLen

uint8 dataLen

samples data length

§ eventIndex

uint8 eventIndex

event number

§ hdr

osal event header

§ iqSamples

void* iqSamples

list of interleaved I/Q samples (list size is dataLen*2)

§ phy

uint8 phy

current phy

§ rssi

uint16 rssi

current rssi

§ rssiAntenna

uint8 rssiAntenna

antenna ID

§ sampleCtrl

uint8 sampleCtrl

sample control - default filtering or RAW_RF

§ sampleRate

uint8 sampleRate

sample rate (1/2/3/4 MHz)

§ sampleSize

uint8 sampleSize

sample size (8 or 16 bit)

§ slotDuration

uint8 slotDuration

sampling slot 1us or 2us

§ status

uint8 status

packet status (success or CRC error)

§ totalDataLen

uint16 totalDataLen

samples data length includes in all next events


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale