TI BLE5-Stack API Documentation  9.14.01
Data Fields
hciEvt_BLEEnhConnComplete_t Struct Reference

LE Enhanced Connection Complete Event. More...

Data Fields

uint8 BLEEventCode
 BLE Event Code. More...
 
uint8 clockAccuracy
 connection clock accuracy More...
 
uint16 connectionHandle
 connection handle More...
 
uint16 connInterval
 connection interval More...
 
uint16 connLatency
 connection latency More...
 
uint16 connTimeout
 connection supervision timeout More...
 
event_hdr_t hdr
 osal event header More...
 
uint8 localRPA [B_ADDR_LEN]
 local resolvable private address More...
 
uint8 peerAddr [B_ADDR_LEN]
 peer address More...
 
uint8 peerAddrType
 peer address type More...
 
uint8 peerRPA [B_ADDR_LEN]
 peer resolvable private address More...
 
uint8 role
 role of connection More...
 
uint8 status
 status of event More...
 

Detailed Description

LE Enhanced Connection Complete Event.

Field Documentation

§ BLEEventCode

uint8 BLEEventCode

BLE Event Code.

§ clockAccuracy

uint8 clockAccuracy

connection clock accuracy

§ connectionHandle

uint16 connectionHandle

connection handle

§ connInterval

uint16 connInterval

connection interval

§ connLatency

uint16 connLatency

connection latency

§ connTimeout

uint16 connTimeout

connection supervision timeout

§ hdr

osal event header

§ localRPA

uint8 localRPA[B_ADDR_LEN]

local resolvable private address

§ peerAddr

uint8 peerAddr[B_ADDR_LEN]

peer address

§ peerAddrType

uint8 peerAddrType

peer address type

§ peerRPA

uint8 peerRPA[B_ADDR_LEN]

peer resolvable private address

§ role

uint8 role

role of connection

§ status

uint8 status

status of event


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale