![]() |
![]() |
|
TI BLE5-Stack API Documentation
9.14.01
|
Host Handover Candidate Node Configuration parameters. More...
Data Fields | |
| uint8_t | appTaskId |
| Application task ID. More... | |
| uint32_t | maxFailedConnEvents |
| uint8_t * | pHandoverData |
| The handover data given by the serving node. More... | |
| uint16_t | rfu |
| Reserved for future use. More... | |
| uint32_t | timeDeltaInUs |
| The time in us it took for the data to be transferred from the serving node to the candidate node. More... | |
| uint32_t | timeDeltaMaxErrInUs |
| The maximum deviation time in us. More... | |
| uint8_t | txBurstRatio |
Host Handover Candidate Node Configuration parameters.
| uint8_t appTaskId |
Application task ID.
| uint32_t maxFailedConnEvents |
Number of connection events the candidate node will try to follow the central When this value is 0, it will try to follow the central device until it reaches supervision timeout
| uint8_t* pHandoverData |
The handover data given by the serving node.
| uint16_t rfu |
Reserved for future use.
| uint32_t timeDeltaInUs |
The time in us it took for the data to be transferred from the serving node to the candidate node.
| uint32_t timeDeltaMaxErrInUs |
The maximum deviation time in us.
| uint8_t txBurstRatio |
Precentage of the connection event the TxBurst will be active. when this value is 0, TxBurst will not be activated.