TI BLE5-Stack API Documentation  9.14.01
Data Fields
gattCharFormat_t Struct Reference

GATT Structure for Characteristic Presentation Format Value. More...

Data Fields

uint16 desc
 Description of this attribute as defined in a higher layer profile. More...
 
int8 exponent
 A sign integer which represents the exponent of an integer. More...
 
uint8 format
 Format of the value of this characteristic. More...
 
uint8 nameSpace
 Name space of the description. More...
 
uint16 unit
 Unit of this attribute as defined in the data dictionary. More...
 

Detailed Description

GATT Structure for Characteristic Presentation Format Value.

Field Documentation

§ desc

uint16 desc

Description of this attribute as defined in a higher layer profile.

§ exponent

int8 exponent

A sign integer which represents the exponent of an integer.

§ format

uint8 format

Format of the value of this characteristic.

§ nameSpace

uint8 nameSpace

Name space of the description.

§ unit

uint16 unit

Unit of this attribute as defined in the data dictionary.


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale