![]() |
![]() |
|
TI BLE5-Stack API Documentation
9.14.01
|
Data Fields | |
| uint8_t | accepted |
| TRUE if host accepts parameter update, FALSE otherwise. More... | |
| uint16_t | connectionHandle |
| Connection handle of the update. More... | |
| uint16_t | connLatency |
| Connection Latency. More... | |
| uint16_t | connTimeout |
| Connection Timeout. More... | |
| uint16_t | intervalMax |
| Maximum Connection Interval. More... | |
| uint16_t | intervalMin |
| Minimum Connection Interval. More... | |
| uint8_t | signalIdentifier |
| L2CAP Signal Identifier. More... | |
Update Link Parameters Request Reply parameters
This is used by GAP_UpdateLinkParamReqReply
| uint8_t accepted |
TRUE if host accepts parameter update, FALSE otherwise.
| uint16_t connectionHandle |
Connection handle of the update.
| uint16_t connLatency |
Connection Latency.
| uint16_t connTimeout |
Connection Timeout.
| uint16_t intervalMax |
Maximum Connection Interval.
| uint16_t intervalMin |
Minimum Connection Interval.
| uint8_t signalIdentifier |
L2CAP Signal Identifier.