TI BLE5-Stack API Documentation  9.14.01
Data Fields
gapPairingReq_t Struct Reference

Data Fields

uint8_t authReq
 Pairing Request Auth Req field. More...
 
uint8_t ioCap
 Pairing Request ioCap field. More...
 
keyDist_t keyDist
 Pairing Request Key Distribution field. More...
 
uint8_t maxEncKeySize
 Pairing Request Maximum Encryption Key Size field. More...
 
uint8_t oobDataFlag
 Pairing Request OOB Data Flag field. More...
 

Detailed Description

Pairing Request fields for GAP_Authenticate which should only be used if the gapbondmgr does not exist

Field Documentation

§ authReq

uint8_t authReq

Pairing Request Auth Req field.

§ ioCap

uint8_t ioCap

Pairing Request ioCap field.

§ keyDist

keyDist_t keyDist

Pairing Request Key Distribution field.

§ maxEncKeySize

uint8_t maxEncKeySize

Pairing Request Maximum Encryption Key Size field.

§ oobDataFlag

uint8_t oobDataFlag

Pairing Request OOB Data Flag field.


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale