TI BLE5-Stack API Documentation  9.14.01
Data Fields
authReq_t Struct Reference

Data Fields

unsigned int bonding:2
 Bonding flags. More...
 
unsigned int ct2:1
 h7 Link Key conversion support (not used in LE) More...
 
unsigned int kp:1
 LE SC Keypress Notifications. More...
 
unsigned int mitm:1
 Man-In-The-Middle (MITM) More...
 
unsigned int reserved:2
 Reserved - don't use. More...
 
unsigned int sc:1
 LE Secure Connections (SC) More...
 

Detailed Description

Pairing Request & Response - authReq field

Field Documentation

§ bonding

unsigned int bonding

Bonding flags.

§ ct2

unsigned int ct2

h7 Link Key conversion support (not used in LE)

§ kp

unsigned int kp

LE SC Keypress Notifications.

§ mitm

unsigned int mitm

Man-In-The-Middle (MITM)

§ reserved

unsigned int reserved

Reserved - don't use.

§ sc

unsigned int sc

LE Secure Connections (SC)


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale