![]() |
![]() |
|
TI BLE5-Stack API Documentation
9.14.01
|
Data type returned with GAP_EVT_SCAN_REQ_RECEIVED event. More...
Data Fields | |
| uint8 | channel |
| Channel when the scan req was received. More... | |
| uint8 | handle |
| Advertising handle. More... | |
| int8 | rssi |
| RSSI of the scan req. More... | |
| uint8 | scanAddr [B_ADDR_LEN] |
| Address of scanning device. More... | |
| uint8 | scanAddrType |
| Address type of scanning device. More... | |
Data type returned with GAP_EVT_SCAN_REQ_RECEIVED event.
| uint8 channel |
Channel when the scan req was received.
| uint8 handle |
Advertising handle.
| int8 rssi |
RSSI of the scan req.
| uint8 scanAddr[B_ADDR_LEN] |
Address of scanning device.
| uint8 scanAddrType |
Address type of scanning device.