TI BLE5-Stack API Documentation  9.14.01
Data Fields
CS_setDefaultSettingsCmdParams_t Struct Reference

Data Fields

uint16_t connHandle
 Connection handle. More...
 
uint8_t csSyncAntennaSelection
 CS sync antenna selection. More...
 
int8_t maxTxPower
 Maximum TX power in dBm. More...
 
uint8_t roleEnable
 Role enable flag. More...
 

Field Documentation

§ connHandle

uint16_t connHandle

Connection handle.

§ csSyncAntennaSelection

uint8_t csSyncAntennaSelection

CS sync antenna selection.

§ maxTxPower

int8_t maxTxPower

Maximum TX power in dBm.

§ roleEnable

uint8_t roleEnable

Role enable flag.


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale