TI BLE5-Stack API Documentation  9.14.01
Data Structures | Macros | Typedefs | Functions
handover.h File Reference

Go to the source code of this file.

Data Structures

struct  handoverCNCBs_t
 Host Handover CN callbacks. More...
 
struct  handoverCNParams_t
 Host Handover Candidate Node Configuration parameters. More...
 
struct  handoverSNCBs_t
 Host Handover SN callbacks. More...
 
struct  handoverSNParams_t
 Host Handover Serving Node Configuration parameters. More...
 

Macros

#define HANDOVER_CONN_ESTABLISH_WITH_HANDOVER   LL_STATUS_ESTABLISH_WITH_HANDOVER
 
#define HANDOVER_CONNHANDLE_INVALID   LL_CONNHANDLE_INVALID
 
#define HANDOVER_DEFAULT_MAX_FAILED_CONN_EVENTS   6
 
#define HANDOVER_HOST_DATA_SIZE   0
 
#define HANDOVER_INVALID_DATA_SIZE   0xFFFFFFFF
 
#define HANDOVER_SN_MODE_DISCONNECT_IMMED   0
 
#define HANDOVER_SN_MODE_WAIT_CN_STATUS   1
 
#define HANDOVER_TX_BURST_RATIO_DEFAULT_VAL   30
 

Typedefs

typedef void(* pfnHandoverStartCNCB_t) (uint16_t connHandle, uint32_t status)
 
typedef void(* pfnHandoverStartSNCB_t) (uint16_t connHandle, uint32_t status)
 

Functions

void Handover_ApplyCnData (uint16_t connHandle)
 
uint8_t Handover_CloseSN (handoverSNParams_t *pParams, uint16_t handoverStatus)
 
uint32_t Handover_GetSNDataSize (handoverSNParams_t *pParams)
 
uint8_t Handover_InitCNParams (handoverCNParams_t *pParams)
 
uint8_t Handover_InitSNParams (handoverSNParams_t *pParams)
 
uint8_t Handover_RegisterCNCBs (const handoverCNCBs_t *pCBs)
 
uint8_t Handover_RegisterSNCBs (const handoverSNCBs_t *pCBs)
 
uint8_t Handover_StartCN (handoverCNParams_t *pParams)
 
uint8_t Handover_StartSN (handoverSNParams_t *pParams)
 

Macro Definition Documentation

§ HANDOVER_CONN_ESTABLISH_WITH_HANDOVER

#define HANDOVER_CONN_ESTABLISH_WITH_HANDOVER   LL_STATUS_ESTABLISH_WITH_HANDOVER

§ HANDOVER_CONNHANDLE_INVALID

#define HANDOVER_CONNHANDLE_INVALID   LL_CONNHANDLE_INVALID

§ HANDOVER_DEFAULT_MAX_FAILED_CONN_EVENTS

#define HANDOVER_DEFAULT_MAX_FAILED_CONN_EVENTS   6

§ HANDOVER_HOST_DATA_SIZE

#define HANDOVER_HOST_DATA_SIZE   0

§ HANDOVER_INVALID_DATA_SIZE

#define HANDOVER_INVALID_DATA_SIZE   0xFFFFFFFF

§ HANDOVER_SN_MODE_DISCONNECT_IMMED

#define HANDOVER_SN_MODE_DISCONNECT_IMMED   0

§ HANDOVER_SN_MODE_WAIT_CN_STATUS

#define HANDOVER_SN_MODE_WAIT_CN_STATUS   1

§ HANDOVER_TX_BURST_RATIO_DEFAULT_VAL

#define HANDOVER_TX_BURST_RATIO_DEFAULT_VAL   30

Typedef Documentation

§ pfnHandoverStartCNCB_t

typedef void(* pfnHandoverStartCNCB_t) (uint16_t connHandle, uint32_t status)

§ pfnHandoverStartSNCB_t

typedef void(* pfnHandoverStartSNCB_t) (uint16_t connHandle, uint32_t status)

Function Documentation

§ Handover_ApplyCnData()

void Handover_ApplyCnData ( uint16_t  connHandle)

§ Handover_CloseSN()

uint8_t Handover_CloseSN ( handoverSNParams_t pParams,
uint16_t  handoverStatus 
)

Handover_CloseSN

Close the Handover process on the serving node side. If the handover was successful this will cause the serving node to teminate the conenction. Otherwise, it will continue the connection with the peer device.

Parameters
pParams- Pointer to the serving node parameters
handoverStatus- TRUE if the candidate was able to follow the handover connection. Otherwise, FALSE
Returns
SUCCESS
bleIncorrectMode
INVALIDPARAMETER

§ Handover_GetSNDataSize()

uint32_t Handover_GetSNDataSize ( handoverSNParams_t pParams)

Handover_GetSNDataSize

Request the controller data size and returns the sum of the controller and host data size

Parameters
pParams- pointer to serving node parameters
connHandle- the connection handle of the requested handover link
Returns
SUCCESS
FAILURE

§ Handover_InitCNParams()

uint8_t Handover_InitCNParams ( handoverCNParams_t pParams)

Handover_InitCNParams

Initialize the given parameter structure with default values

Parameters
pParams- Pointer to the parameters structure
Returns
SUCCESS
FAILURE

§ Handover_InitSNParams()

uint8_t Handover_InitSNParams ( handoverSNParams_t pParams)

Handover_InitSNParams

Initialize the given parameter structure with default values

Parameters
pParams- Pointer to the parameters structure
Returns
SUCCESS
FAILURE

§ Handover_RegisterCNCBs()

uint8_t Handover_RegisterCNCBs ( const handoverCNCBs_t pCBs)

Handover_RegisterCNCBs

Register the application callback function at the host

Parameters
pCBs- pointer to the callback functions
Returns
SUCCESS
FAILURE

§ Handover_RegisterSNCBs()

uint8_t Handover_RegisterSNCBs ( const handoverSNCBs_t pCBs)

Handover_RegisterSNCBs

Register the application callback function at the host

Parameters
pCBs- pointer to the callback functions
Returns
SUCCESS
FAILURE

§ Handover_StartCN()

uint8_t Handover_StartCN ( handoverCNParams_t pParams)

Handover_StartCN

Starts the Handover process on the serving node side. This function will save the application data size and will call the LL command for further handling

: BLE_LOKI-1495

Parameters
pParams- Pointer to the candidate node parameters
Returns
SUCCESS
bleNoResources
bleAlreadyInRequestedMode
bleInvalidRange
LL_STATUS_SUCCESS
LL_STATUS_ERROR_CONNECTION_LIMIT_EXCEEDED
LL_STATUS_ERROR_COMMAND_DISALLOWED
LL_STATUS_ERROR_BAD_PARAMETER

§ Handover_StartSN()

uint8_t Handover_StartSN ( handoverSNParams_t pParams)

Handover_StartSN

Starts the Handover process on the serving node side. This function will save the application data size and will call the LL command for further handling

Parameters
pParams- Pointer to the serving node parameters
Returns
SUCCESS
bleIncorrectMode
bleNotConnected
bleAlreadyInRequestedMode
INVALIDPARAMETER
LL_STATUS_SUCCESS
LL_STATUS_ERROR_INACTIVE_CONNECTION
LL_STATUS_ERROR_COMMAND_DISALLOWED
LL_STATUS_ERROR_BAD_PARAMETER
LL_STATUS_ERROR_DUE_TO_LIMITED_RESOURCES

NOTE: The caller is responsible to free the pBuf upon failure.

© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale