TI BLE5-Stack API Documentation  9.14.01
Macros

Macros

#define ATT_ERR_ATTR_NOT_FOUND   0x0a
 No attribute found within the given attribute handle range. More...
 
#define ATT_ERR_ATTR_NOT_LONG   0x0b
 Attribute cannot be read or written using the Read Blob Request or Prepare Write Request. More...
 
#define ATT_ERR_INSUFFICIENT_AUTHEN   0x05
 The attribute requires authentication before it can be read or written. More...
 
#define ATT_ERR_INSUFFICIENT_AUTHOR   0x08
 The attribute requires an authorization before it can be read or written. More...
 
#define ATT_ERR_INSUFFICIENT_ENCRYPT   0x0f
 The attribute requires encryption before it can be read or written. More...
 
#define ATT_ERR_INSUFFICIENT_KEY_SIZE   0x0c
 The Encryption Key Size used for encrypting this link is insufficient. More...
 
#define ATT_ERR_INSUFFICIENT_RESOURCES   0x11
 Insufficient Resources to complete the request. More...
 
#define ATT_ERR_INVALID_HANDLE   0x01
 Attribute handle value given was not valid on this attribute server. More...
 
#define ATT_ERR_INVALID_OFFSET   0x07
 Offset specified was past the end of the attribute. More...
 
#define ATT_ERR_INVALID_PDU   0x04
 The attribute PDU was invalid. More...
 
#define ATT_ERR_INVALID_VALUE   0x80
 The attribute value is invalid for the operation. More...
 
#define ATT_ERR_INVALID_VALUE_SIZE   0x0d
 The attribute value length is invalid for the operation. More...
 
#define ATT_ERR_PREPARE_QUEUE_FULL   0x09
 Too many prepare writes have been queued. More...
 
#define ATT_ERR_READ_NOT_PERMITTED   0x02
 Attribute cannot be read. More...
 
#define ATT_ERR_UNLIKELY   0x0e
 The attribute request that was requested has encountered an error that was very unlikely, and therefore could not be completed as requested. More...
 
#define ATT_ERR_UNSUPPORTED_GRP_TYPE   0x10
 The attribute type is not a supported grouping attribute as defined by a higher layer specification. More...
 
#define ATT_ERR_UNSUPPORTED_REQ   0x06
 Attribute server doesn't support the request received from the attribute client. More...
 
#define ATT_ERR_WRITE_NOT_PERMITTED   0x03
 Attribute cannot be written. More...
 

Detailed Description

Macro Definition Documentation

§ ATT_ERR_ATTR_NOT_FOUND

#define ATT_ERR_ATTR_NOT_FOUND   0x0a

No attribute found within the given attribute handle range.

§ ATT_ERR_ATTR_NOT_LONG

#define ATT_ERR_ATTR_NOT_LONG   0x0b

Attribute cannot be read or written using the Read Blob Request or Prepare Write Request.

§ ATT_ERR_INSUFFICIENT_AUTHEN

#define ATT_ERR_INSUFFICIENT_AUTHEN   0x05

The attribute requires authentication before it can be read or written.

§ ATT_ERR_INSUFFICIENT_AUTHOR

#define ATT_ERR_INSUFFICIENT_AUTHOR   0x08

The attribute requires an authorization before it can be read or written.

§ ATT_ERR_INSUFFICIENT_ENCRYPT

#define ATT_ERR_INSUFFICIENT_ENCRYPT   0x0f

The attribute requires encryption before it can be read or written.

§ ATT_ERR_INSUFFICIENT_KEY_SIZE

#define ATT_ERR_INSUFFICIENT_KEY_SIZE   0x0c

The Encryption Key Size used for encrypting this link is insufficient.

§ ATT_ERR_INSUFFICIENT_RESOURCES

#define ATT_ERR_INSUFFICIENT_RESOURCES   0x11

Insufficient Resources to complete the request.

§ ATT_ERR_INVALID_HANDLE

#define ATT_ERR_INVALID_HANDLE   0x01

Attribute handle value given was not valid on this attribute server.

§ ATT_ERR_INVALID_OFFSET

#define ATT_ERR_INVALID_OFFSET   0x07

Offset specified was past the end of the attribute.

§ ATT_ERR_INVALID_PDU

#define ATT_ERR_INVALID_PDU   0x04

The attribute PDU was invalid.

§ ATT_ERR_INVALID_VALUE

#define ATT_ERR_INVALID_VALUE   0x80

The attribute value is invalid for the operation.

§ ATT_ERR_INVALID_VALUE_SIZE

#define ATT_ERR_INVALID_VALUE_SIZE   0x0d

The attribute value length is invalid for the operation.

§ ATT_ERR_PREPARE_QUEUE_FULL

#define ATT_ERR_PREPARE_QUEUE_FULL   0x09

Too many prepare writes have been queued.

§ ATT_ERR_READ_NOT_PERMITTED

#define ATT_ERR_READ_NOT_PERMITTED   0x02

Attribute cannot be read.

§ ATT_ERR_UNLIKELY

#define ATT_ERR_UNLIKELY   0x0e

The attribute request that was requested has encountered an error that was very unlikely, and therefore could not be completed as requested.

§ ATT_ERR_UNSUPPORTED_GRP_TYPE

#define ATT_ERR_UNSUPPORTED_GRP_TYPE   0x10

The attribute type is not a supported grouping attribute as defined by a higher layer specification.

§ ATT_ERR_UNSUPPORTED_REQ

#define ATT_ERR_UNSUPPORTED_REQ   0x06

Attribute server doesn't support the request received from the attribute client.

§ ATT_ERR_WRITE_NOT_PERMITTED

#define ATT_ERR_WRITE_NOT_PERMITTED   0x03

Attribute cannot be written.

© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale