TI BLE5-Stack API Documentation  9.14.01
Data Structures | Macros | Typedefs | Functions
gapgattserver.h File Reference

Detailed Description

GAP Attribute Server interface

Go to the source code of this file.

Data Structures

struct  ggsAppCBs_t
 

Macros

#define GAP_DEVICE_NAME_LEN   31
 Length of Device Name Attribute value excluding null-terminate char. More...
 
#define GAP_PRIVACY_DISABLED   0x00
 Central Address Resolution: Privacy is Disabled. More...
 
#define GAP_PRIVACY_ENABLED   0x01
 Central Address Resolution: Privacy is Enabled. More...
 
#define GAP_RPA_ONLY_MODE   0x00
 Only Resolvable Private Addresses Shall Be Used. More...
 
#define GGS_APPEARANCE_ATT   1
 
#define GGS_CENT_ADDR_RES_ATT   9
 
#define GGS_DEVICE_NAME_ATT   0
 
#define GGS_PERI_CONN_PARAM_ATT   4
 
#define GGS_RESOLVABLE_PRIVATE_ADDRESS_ONLY_ATT   10
 

Typedefs

typedef void(* ggsAttrValueChange_t) (uint16 connHandle, uint8 attrId)
 Callback to notify when attribute value is changed over the air. More...
 

Functions

bStatus_t GGS_AddService (uint32 services)
 
bStatus_t GGS_DelService (uint32 services)
 
bStatus_t GGS_GetParameter (uint8 param, void *value)
 
uint16 GGS_GetParamValue (void)
 
void GGS_RegisterAppCBs (ggsAppCBs_t *appCallbacks)
 
bStatus_t GGS_SetParameter (uint8 param, uint8 len, void *value)
 
void GGS_SetParamValue (uint16 value)
 
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale