Changelog
Table of Contents
New Features
BLE Stack
| ID | Summary |
|---|---|
| BLE_LOKI-3836 | Add Connection Parameter Update Event Handler to Car Node Example |
| BLE_LOKI-3819 | Reduce the Number of Steps within TX Double Buffer for Channel Sounding |
| BLE_LOKI-3801 | Add Connection Parameter Update APIs |
| BLE_LOKI-3798 | Implement RAS/RAP Real Time Client |
| BLE_LOKI-3786 | Add Support for L2CAP Send SDU Flow Control with Channel Sounding |
| BLE_LOKI-3754 | Support Central Mode on Key Node Example |
| BLE_LOKI-3629 | Support Initializing of Multiple Generated Advertising Sets in SysConfig |
TI Proprietary RF
| ID | Summary |
|---|---|
| None | None |
TI Zigbee
| ID | Summary |
|---|---|
| None | None |
SimpleLink Common Commponents Module (SCCM)
| ID | Summary |
|---|---|
| SCCM-592 | CC27XX HSM BareMetal module shall support Asymmetric Asset operations |
| SCCM-591 | CC27XX HSM BareMetal Module shall support one key blob element |
Core SDK
| ID | Summary |
|---|---|
| LPRFXXWARE-1072 | Add UART2 LIN HAL-support |
Radio Control Library (RCL)
| ID | Summary |
|---|---|
| RCL-1257 | BLE CS: Improve Tx tone quality for multiple antenna configuration |
Fixed Issues
BLE Stack
| ID | Summary |
|---|---|
| BLE_LOKI-3849 | Reject Connection Parameter Update Request from Peer during CS Procedure |
| BLE_LOKI-3840 | Scanner cannot Find Device that Distributes IRK with Static Random Address after Bonding and Reset |
| BLE_LOKI-3837 | Fix Synchronization - Procedure Counter not Incremented when Reject Packet Sent/Received |
| BLE_LOKI-3820 | Adjust Peripheral startTime in Case we Miss the Peer on the CS Instant |
| BLE_LOKI-3808 | Repeated calls to CS_GetRole floods the BLE Stack message queue |
| BLE_LOKI-3807 | Scheduling Stops when Device Disconnects During Channel Sounding |
| BLE_LOKI-3800 | Channel Sounding may Lose Synchronization of Procedure Counter when Multiple Tasks are Active |
| BLE_LOKI-3795 | BLE Stack Might Hang when Adv/Scan Executes Before the CS Procedure |
| BLE_LOKI-3794 | Channel Sounding CS_SUBEVENT may Report Incorrect Connection Handle |
| BLE_LOKI-3793 | BLE Stack Scheduler Time Comparison Causes Channel Sounding to Crash |
| BLE_LOKI-3790 | Large CS_OFFSET Value Causes Reflector to Miss the Start Procedure |
| BLE_LOKI-3789 | Bluetooth Health Thermometer Profile uses Incorrect Data Format |
| BLE_LOKI-3788 | No GAP_EVT_SCAN_ENABLED Events when only Selected Observer Role in SysCfg |
TI Proprietary RF
| ID | Summary |
|---|---|
| None | None |
TI Zigbee
| ID | Summary |
|---|---|
| TI_ZIGBEE-260 | Hardcoded 50ms delay between fragmented packets |
SimpleLink Common Commponents Module (SCCM)
| ID | Summary |
|---|---|
| SCCM-621 | Extra trailer length of 0x630 getting introduced |
Core SDK
| ID | Summary |
|---|---|
| TIDRIVERS-7596 | APULPF3_dataMemTransfer fails when source and destination is in APU memory |
Radio Control Library (RCL)
| ID | Summary |
|---|---|
| None | None |
Known Issues
BLE Stack
| ID | Summary |
|---|---|
| BLE_LOKI-3872 | Distance not Reported for One or More Keys During Multiple Connections |
| BLE_LOKI-3869 | Looping Through CM Start and CM Stop Causes Channel Sounding Failure |
| BLE_LOKI-3828 | CS Procedure may be Aborted if Received Data Length/Time Exceeds CS_OFFSET |
| BLE_LOKI-3724 | IAR Compiler Error when Compiling Basic_persistent on CC2340 Devices |
| BLE_LOKI-3676 | Channel Sounding Timeout Distance Events for Mode 3 with 2x2 Antennas |
| BLE_LOKI-3536 | If parameter update or channel map update w/ CSA#1 is from the past - Connection Monitor will terminate |
| BLE_LOKI-3535 | Connection Monitor Cannot properly track connection on Coded PHY |
| BLE_LOKI-3473 | IAR Compiled Car Node and Key Node Executing Channel Sounding in Loops Causes GAP Link Termination |
| BLE_LOKI-3429 | No Distance is Received after 160 to 255 CS Procedures using RAS over Indications |
| BLE_LOKI-3389 | CS procedure must be complete before starting the next one |
| BLE_LOKI-3236 | Calling HCI_ResetCmd Causes Program to Crash |
| BLE_LOKI-3208 | BLE Agent GUI not able to calculate time offset correctly when running connection handover demo which causes frequent unsuccessful handover sessions |
| BLE_LOKI-3177 | [SWAT] Observer failed to receive GAP_EVT_SCAN_DISABLED event |
| BLE_LOKI-3097 | After changing PHY both devices continue to send Power Reporting events |
| BLE_LOKI-2978 | Connnection Handover AuthenticationComplete Event Received after Handover When Candidate Configured To Initiate Pairing Request |
| BLE_LOKI-2842 | CC23XX and CC27XX family of devices rounds down Tx power values that are not in the power table |
| BLE_LOKI-2650 | CC2745R10Q1 Central Role Fails to Switch Connection PHY to Coded While Holding 16 Connections |
| BLE_LOKI-2648 | Connection may be unstable with Coded PHY when Access Address has high cross-correlation with the preamble |
| BLE_LOKI-2373 | CC2340R5 MAX periodic adv list size is hard coded and can't be configure by SysConfig |
| BLE_LOKI-2358 | CC2340R5 Basic MR printed peripheral initial RPA after bond and pair, instead of its Public Address |
| BLE_LOKI-2108 | Specific smart phone doesn't find peer running extended ADV with secondary PHY of 1M |
| BLE_LOKI-1630 | Extended Advertisement Reports Are Not Filtered When SCAN_PARAM_FLT_DUP is Enabled |
TI Proprietary RF
| ID | Summary |
|---|---|
| None | None |
TI Zigbee
| ID | Summary |
|---|---|
| None | None |
SimpleLink Common Commponents Module (SCCM)
| ID | Summary |
|---|---|
| None | None |
Core SDK
| ID | Summary |
|---|---|
| TIDRIVERS-7475 | I2S driver should not be used simultaneously with CAN or APU driver |
| TIDRIVERS-7416 | The Power driver does not handle SysTimer channel 5 for CC27XX |
| TIDRIVERS-7244 | Changing the muxing on an IO can cause glitches under some conditions |
| TIDRIVERS-7234 | FPU registers not saved/restored around standby for NoRTOS/CM33 |
| TIDRIVERS-7016 | AESCCM/AESGCM driver do not support segmented finalize with no input when using HSM engine for CC27XX devices |
| TIDRIVERS-6863 | JSON library unstable for gcc 12.3 |
| LPRFSEC-250 | PSA EDDSA+AES CBC,CCM,GCM,CMAC,CTR lack concurrent operation support |
Radio Control Library (RCL)
| ID | Summary |
|---|---|
| None | None |