API Documentation  9.14.01
Macros used to configure GPIO pins

GPIO_PinConfig output pin configuration macros

#define GPIO_CFG_OUTPUT
 
#define GPIO_CFG_OUT_STD
 
#define GPIO_CFG_OUT_OD_NOPULL
 
#define GPIO_CFG_OUT_OD_PU
 
#define GPIO_CFG_OUT_OD_PD
 
#define GPIO_CFG_OUT_STR_LOW
 
#define GPIO_CFG_OUT_STR_MED
 
#define GPIO_CFG_OUT_STR_HIGH
 
#define GPIO_CFG_OUT_HIGH
 
#define GPIO_CFG_OUT_LOW
 

GPIO_PinConfig input pin configuration macros

#define GPIO_CFG_INPUT
 
#define GPIO_CFG_IN_NOPULL
 
#define GPIO_CFG_IN_PU
 
#define GPIO_CFG_IN_PD
 

GPIO_PinConfig nondirectional pin configuration macros

#define GPIO_CFG_NO_DIR
 

GPIO_PinConfig pin inversion configuration macros

#define GPIO_CFG_INVERT_OFF
 
#define GPIO_CFG_INVERT_ON
 

GPIO_PinConfig pin hysteresis configuration macros

#define GPIO_CFG_HYSTERESIS_OFF
 
#define GPIO_CFG_HYSTERESIS_ON
 

GPIO_PinConfig slew rate configuration macros

#define GPIO_CFG_SLEW_NORMAL
 
#define GPIO_CFG_SLEW_REDUCED
 

GPIO_PinConfig interrupt configuration macros

#define GPIO_CFG_IN_INT_NONE
 
#define GPIO_CFG_IN_INT_FALLING
 
#define GPIO_CFG_IN_INT_RISING
 
#define GPIO_CFG_IN_INT_BOTH_EDGES
 
#define GPIO_CFG_IN_INT_LOW
 
#define GPIO_CFG_IN_INT_HIGH
 
#define GPIO_CFG_INT_DISABLE
 
#define GPIO_CFG_INT_ENABLE
 

GPIO_PinConfig power mode configuration macros

For devices that support low power modes, standard GPIO interrupts may be disabled in some modes. These defines allow configuring individual pins as wake-up sources. The GPIO module's wake up configuration is always enabled if it exists, so there is no module-level configuration. See the device-specific header files for details.

#define GPIO_CFG_SHUTDOWN_WAKE_OFF
 
#define GPIO_CFG_SHUTDOWN_WAKE_HIGH
 
#define GPIO_CFG_SHUTDOWN_WAKE_LOW
 

GPIO_pinconfig macro preventing configuration

Should be used if a pin is configured before the first GPIO_init() call, and should not be overwritten

#define GPIO_CFG_DO_NOT_CONFIG
 

GPIO_Mux configuration macros

For additional muxing options, see the directions in the device-specific GPIO driver.

#define GPIO_MUX_GPIO
 

Detailed Description

Macro Definition Documentation

§ GPIO_CFG_DO_NOT_CONFIG

#define GPIO_CFG_DO_NOT_CONFIG

Prevent this GPIO from being configured by the GPIO driver

§ GPIO_CFG_HYSTERESIS_OFF

#define GPIO_CFG_HYSTERESIS_OFF

Input hysteresis is disabled (default)

§ GPIO_CFG_HYSTERESIS_ON

#define GPIO_CFG_HYSTERESIS_ON

Input hysteresis is enabled

§ GPIO_CFG_IN_INT_BOTH_EDGES

#define GPIO_CFG_IN_INT_BOTH_EDGES

Interrupt on both edges

§ GPIO_CFG_IN_INT_FALLING

#define GPIO_CFG_IN_INT_FALLING

Interrupt on falling edge

§ GPIO_CFG_IN_INT_HIGH

#define GPIO_CFG_IN_INT_HIGH

Interrupt on high level

§ GPIO_CFG_IN_INT_LOW

#define GPIO_CFG_IN_INT_LOW

Interrupt on low level

§ GPIO_CFG_IN_INT_NONE

#define GPIO_CFG_IN_INT_NONE

No Interrupt (default)

§ GPIO_CFG_IN_INT_RISING

#define GPIO_CFG_IN_INT_RISING

Interrupt on rising edge

§ GPIO_CFG_IN_NOPULL

#define GPIO_CFG_IN_NOPULL

Input pin with no internal PU/PD

§ GPIO_CFG_IN_PD

#define GPIO_CFG_IN_PD

Input pin with internal PD

§ GPIO_CFG_IN_PU

#define GPIO_CFG_IN_PU

Input pin with internal PU

§ GPIO_CFG_INPUT

#define GPIO_CFG_INPUT

Pin is an input.

§ GPIO_CFG_INT_DISABLE

#define GPIO_CFG_INT_DISABLE

Interrupt disabled (default)

§ GPIO_CFG_INT_ENABLE

#define GPIO_CFG_INT_ENABLE

Interrupt enabled

§ GPIO_CFG_INVERT_OFF

#define GPIO_CFG_INVERT_OFF

Input/output values are normal (default)

§ GPIO_CFG_INVERT_ON

#define GPIO_CFG_INVERT_ON

Input/output values are inverted

§ GPIO_CFG_NO_DIR

#define GPIO_CFG_NO_DIR

Input and output are both disabled. Primarily useful for disabling muxed pins.

§ GPIO_CFG_OUT_HIGH

#define GPIO_CFG_OUT_HIGH

Set pin's output to 1.

§ GPIO_CFG_OUT_LOW

#define GPIO_CFG_OUT_LOW

Set pin's output to 0.

§ GPIO_CFG_OUT_OD_NOPULL

#define GPIO_CFG_OUT_OD_NOPULL

Output pin is Open Drain

§ GPIO_CFG_OUT_OD_PD

#define GPIO_CFG_OUT_OD_PD

Output pin is Open Drain w/ pull dn

§ GPIO_CFG_OUT_OD_PU

#define GPIO_CFG_OUT_OD_PU

Output pin is Open Drain w/ pull up

§ GPIO_CFG_OUT_STD

#define GPIO_CFG_OUT_STD

Output pin is actively driven high and low

§ GPIO_CFG_OUT_STR_HIGH

#define GPIO_CFG_OUT_STR_HIGH

Set output pin strength to high

§ GPIO_CFG_OUT_STR_LOW

#define GPIO_CFG_OUT_STR_LOW

Set output pin strength to low

§ GPIO_CFG_OUT_STR_MED

#define GPIO_CFG_OUT_STR_MED

Set output pin strength to medium

§ GPIO_CFG_OUTPUT

#define GPIO_CFG_OUTPUT

Pin is an output. Equivalent to OUT_STD.

§ GPIO_CFG_SHUTDOWN_WAKE_HIGH

#define GPIO_CFG_SHUTDOWN_WAKE_HIGH

A high value will wake the device from shutdown

§ GPIO_CFG_SHUTDOWN_WAKE_LOW

#define GPIO_CFG_SHUTDOWN_WAKE_LOW

A low value will wake the device from shutdown

§ GPIO_CFG_SHUTDOWN_WAKE_OFF

#define GPIO_CFG_SHUTDOWN_WAKE_OFF

This pin will not wake the device up

§ GPIO_CFG_SLEW_NORMAL

#define GPIO_CFG_SLEW_NORMAL

Output slew rate is unchanged (default)

§ GPIO_CFG_SLEW_REDUCED

#define GPIO_CFG_SLEW_REDUCED

Output slew rate is reduced

§ GPIO_MUX_GPIO

#define GPIO_MUX_GPIO

Set this pin to be a GPIO (the default)