|
TI OAD API Documentation
9.14.01
|
Functions | |
| psa_status_t | psa_get_key_attributes (psa_key_id_t key, psa_key_attributes_t *attributes) |
| void | psa_reset_key_attributes (psa_key_attributes_t *attributes) |
| psa_status_t psa_get_key_attributes | ( | psa_key_id_t | key, |
| psa_key_attributes_t * | attributes | ||
| ) |
Retrieve the attributes of a key.
This function first resets the attribute structure as with psa_reset_key_attributes(). It then copies the attributes of the given key into the given attribute structure.
| [in] | key | Identifier of the key to query. |
| [in,out] | attributes | On success, the attributes of the key. On failure, equivalent to a freshly-initialized structure. |
| #PSA_SUCCESS | |
| #PSA_ERROR_INVALID_HANDLE | |
| #PSA_ERROR_INSUFFICIENT_MEMORY | |
| #PSA_ERROR_COMMUNICATION_FAILURE | |
| #PSA_ERROR_CORRUPTION_DETECTED | |
| #PSA_ERROR_STORAGE_FAILURE | |
| #PSA_ERROR_DATA_CORRUPT | |
| #PSA_ERROR_DATA_INVALID | |
| #PSA_ERROR_BAD_STATE | The library has not been previously initialized by psa_crypto_init(). It is implementation-dependent whether a failure to initialize results in this error code. |
| void psa_reset_key_attributes | ( | psa_key_attributes_t * | attributes | ) |
Reset a key attribute structure to a freshly initialized state.
You must initialize the attribute structure as described in the documentation of the type #psa_key_attributes_t before calling this function. Once the structure has been initialized, you may call this function at any time.
This function frees any auxiliary resources that the structure may contain.
| [in,out] | attributes | The attribute structure to reset. |
1.8.12