|
TI OAD API Documentation
9.14.01
|
Contains common structures and defines related to external flash layout as it for the OAD usecase. More...
Go to the source code of this file.
Macros | |
| #define | EFL_ADDR_META 0x00000 |
| #define | EFL_ADDR_META_FACT_IMG EFL_ADDR_META |
| #define | EFL_FACT_IMG_META_PG 0 |
| #define | EFL_IMG_STR_ADDR_OFFSET offsetof(ExtImageInfo_t, extFlAddr) |
| #define | EFL_META_COPY_SZ offsetof(ExtImageInfo_t, fixedHdr.rfu) + sizeof(((ExtImageInfo_t){0}).fixedHdr.rfu) |
| #define | EFL_META_COUNTER_OFFSET offsetof(ExtImageInfo_t, counter) |
| #define | EFL_META_PG_INVALID 0xFF |
| #define | EFL_METADATA_LEN sizeof(ExtImageInfo_t) |
| #define | EFL_SIZE_META EFL_PAGE_SIZE |
| #define | OAD_EFL_MAGIC |
| #define | OAD_EFL_MAGIC_SZ 8 |
Variables | |
| uint32_t | counter |
| Timestamp/counter of image. | |
| uint32_t | extFlAddr |
| Location of the image in ext flash. | |
| ExtImageInfo_t | |
| TYPEDEF_STRUCT_PACKED | |
| This is the core image header. More... | |
Contains common structures and defines related to external flash layout as it for the OAD usecase.
1.8.12