TI BLE5-Stack API Documentation  9.14.01
Data Fields
l2capSignalEvent_t Struct Reference

OSAL L2CAP_SIGNAL_EVENT message format. More...

Data Fields

l2capSignalCmd_t cmd
 command data More...
 
uint16 connHandle
 connection message was received on More...
 
osal_event_hdr_t hdr
 L2CAP_SIGNAL_EVENT and status. More...
 
uint8 id
 identifier to match responses with requests More...
 
uint8 opcode
 type of command: L2CAP Signaling Codes (type of commands) More...
 

Detailed Description

OSAL L2CAP_SIGNAL_EVENT message format.

This message is used to deliver an incoming Signaling command up to an upper layer application.

Field Documentation

§ cmd

command data

§ connHandle

uint16 connHandle

connection message was received on

§ hdr

L2CAP_SIGNAL_EVENT and status.

§ id

uint8 id

identifier to match responses with requests

§ opcode

uint8 opcode

The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale