TI BLE5-Stack API Documentation  9.14.01
Data Fields
hciEvt_BLECteRequestFailed_t Struct Reference

LE CTE Request Failed Event. More...

Data Fields

uint8 BLEEventCode
 BLE Event Code. More...
 
uint16 connHandle
 connection handle More...
 
event_hdr_t hdr
 osal event header More...
 
uint8 status
 status More...
 

Detailed Description

LE CTE Request Failed Event.

Field Documentation

§ BLEEventCode

uint8 BLEEventCode

BLE Event Code.

§ connHandle

uint16 connHandle

connection handle

§ hdr

osal event header

§ status

uint8 status

status


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale