TI BLE5-Stack API Documentation  9.14.01
Data Fields
hciEvt_BLECteConnectionIqReport_t Struct Reference

LE CTE Connection IQ Report Event. More...

Data Fields

uint8 BLEEventCode
 BLE Event Code. More...
 
uint16 connEvent
 connection event More...
 
uint16 connHandle
 connection handle More...
 
uint8 cteType
 cte type More...
 
uint8 dataChIndex
 index of data channel More...
 
event_hdr_t hdr
 osal event header More...
 
int8 * iqSamples
 list of interleaved I/Q samples More...
 
uint8 phy
 current phy More...
 
uint16 rssi
 current rssi More...
 
uint8 rssiAntenna
 antenna ID More...
 
uint8 sampleCount
 number of samples More...
 
uint8 slotDuration
 sampling slot 1us or 2us More...
 
uint8 status
 packet status (success or CRC error) More...
 

Detailed Description

LE CTE Connection IQ Report Event.

Field Documentation

§ BLEEventCode

uint8 BLEEventCode

BLE Event Code.

§ connEvent

uint16 connEvent

connection event

§ connHandle

uint16 connHandle

connection handle

§ cteType

uint8 cteType

cte type

§ dataChIndex

uint8 dataChIndex

index of data channel

§ hdr

osal event header

§ iqSamples

int8* iqSamples

list of interleaved I/Q samples

§ phy

uint8 phy

current phy

§ rssi

uint16 rssi

current rssi

§ rssiAntenna

uint8 rssiAntenna

antenna ID

§ sampleCount

uint8 sampleCount

number of samples

§ slotDuration

uint8 slotDuration

sampling slot 1us or 2us

§ status

uint8 status

packet status (success or CRC error)


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale